FlashLoader for 1021?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FlashLoader for 1021?

1,552 次查看
JesseCronce
Contributor I

Hello! I downloaded the flashloader application as a starting point for a custom bootloader for a 1021 project. When I try to build the example loader I get

section `.text' will not fit in region `m_text'
m_text: 96280 B 87 KB 108.07%
c:/nxp/mcuxpressoide_11.1.0_3209/ide/plugins/com.nxp.mcuxpresso.tools.win32_11.1.0.201909161352/tools/bin/../lib/gcc/arm-none-eabi/8.3.1/../../../../arm-none-eabi/bin/ld.exe: region `m_text' overflowed by 7192 bytes

Is there a different or updated version of a bootloader/flash writer that will build for this processor? I have to make modifications to this application anyway, but I would prefer to start with a working image if I could and make changes from there. I would have hoped the example projects would build.

Also, is there any sort of application guide for this software? I found a few posts on the topic, but if there was something in the way of a usage or commissioning or application manual, that would be such a help to me!

Thanks in advance!

0 项奖励
回复
2 回复数

1,539 次查看
b36401
NXP Employee
NXP Employee

Please try to increase m_text region size in linker file.

0 项奖励
回复

1,531 次查看
JesseCronce
Contributor I

The m_text size is set to what is available for this chip. I can get the software to build by building for release, but I was hoping to be able to build for debug and print to the debug console. The release code runs as expected. Again, I was hoping to be able to interact with the board more with debug features.

0 项奖励
回复