Flash Android 10 Dual Bootloader on IMX8MM with 8G eMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash Android 10 Dual Bootloader on IMX8MM with 8G eMMC

5,407 Views
jarvis_tsai
Contributor I

Hi NXP support team,

I am using IMX8M mini cpu and try to flash dual bootloader on our 8G eMMc board.

However there are not ".bpt file" for "7GB dual-bootloader" in "device/fsl/common/partition".

 pastedImage_1.png

So i create and modify one for "7GB" based on "device-partitions-13GB-ab-dual-bootloader.bpt".

You can see attached .btp file and the patch i modified like below.
@@ -1,6 +1,6 @@
{
"settings": {
- "disk_size": "13 GiB",
+ "disk_size": "7 GiB",
"disk_alignment": 2097152,
"first_partition_offset": 8388608
},
@@ -54,14 +54,14 @@
{
"ab": true,
"label": "vendor",
- "size": "512 MiB",
+ "size": "256 MiB",
"guid": "auto",
"type_guid": "2578eab2-a534-43e2-92c0-fed1b01c5d1d"
},
{
"ab": true,
"label": "product",
- "size": "1792 MiB",
+ "size": "896 MiB",
"guid": "auto",
"type_guid": "c1dedb9a-a0d3-42e4-b74d-0acf96833624"
},

After i build and try to flsah image with command ".\uuu_imx_android_flash.bat -f imx8mm -a -c 7 -u dual".

It always fails in flashing "vendor.img" like below :

dual bootloader is supported
dtbo is supported
dual slot is supported
generate lines to flash spl-imx8mm-dual.bin to the partition of bootloader0
generate lines to flash partition-table-dual.img to the partition of gpt
generate lines to flash bootloader-imx8mm-dual.img to the partition of bootloader_a
generate lines to flash dtbo-imx8mm.img to the partition of dtbo_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash system.img to the partition of system_a
generate lines to flash vendor.img to the partition of vendor_a
generate lines to flash product.img to the partition of product_a
generate lines to flash vbmeta-imx8mm.img to the partition of vbmeta_a
uuu script generated, start to invoke uuu with the generated uuu script
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.3.171-0-g4249f93

Success 0 Failure 1


1:13 15/22 [Request would exceed partition size! ] FB: flash vendor_a vendor.img.link

I also modify vendor size to 512 MiB in .btp file, but it still fails as above.   

{
"ab": true,
"label": "vendor",
"size": "512 MiB",
"guid": "auto",
"type_guid": "2578eab2-a534-43e2-92c0-fed1b01c5d1d"
},

My vendor.img only has 69,073 KB.

Please help to create a "7GB dual-bootloader" .btp file to flash. 

Thanks.

Labels (1)
0 Kudos
Reply
2 Replies

5,221 Views
jarvis_tsai
Contributor I

Hi Igor,

I check the document you provided and i still flash failed.

After i test several times i found something may be the root cause.

Here are my tests :

1. I modify a "7GB dual-bootloader" .bpt file based on "13GB dual-bootloader" one (I only change "disk_size: 13 GiB" to "disk_size: 7 GiB").

2. I build failed because the sum of capacity in "7GB dual-bootloader" .bpt file is bigger than 7GB.

3. So I modify the "product" size from "1792 MiB" to "896 MiB" in the "7GB dual-bootloader" .bpt file and i can build it.

4. Then I flash image by UUU, it failed on flashing "product.img".

    The error log shows "16/22 [Request would exceed partition size!  ] FB: flash product_a product.img.link".

5. And I try to adjust the capacity of "system", "vendor" and "product" in the "7GB dual-bootloader" .bpt file and it all flash failed.

So I think the size of partition is the root cause, but I can't create a useful "7GB dual-bootloader" .bpt file.

Please help to modify a "7GB dual-bootloader" .bpt file for 8G eMMC.

Btw, it will build failed when enable "IMX_NO_PRODUCT_PARTITION := true", even on "evk_8mm" platform.

Please check this in NXP Android 10 BSP.

Thanks.

0 Kudos
Reply

5,220 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jarvis

for changing partition size one can try to follow sect.8.8.2 Changing the partition size

attached Android Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply