FirstStageMount Fail?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FirstStageMount Fail?

11,324件の閲覧回数
ThanarajS
Contributor III

Hi All,

I am using AOSP9 and IMX6Q SABRESD Board. and I build the source and trying to boot from eMMC. 

Facing issue in fstab mounting point. please find below error logs,

LOG:

=================================================================

U-Boot 2018.03 (Jan 29 2020 - 15:33:22 +0530)

CPU: Freescale i.MX6Q rev1.3 996 MHz (running at 792 MHz)
CPU: Extended Commercial temperature grade (-20C to 105C) at 38C
Reset cause: WDOG
Model: IMX6Q 9.0 Board
Board: IMX6Q SABRESD
DRAM: 2 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... *** Warning - bad CRC, using default environment

Failed (-5)
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
flash target is MMC:2
Net:
Error: ethernet@02188000 address not set.
No ethernet found.
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 3 2 1 0
RNG already instantiated 0x40000003
RNG already instantiated 0x40000003
verify OK, boot 'boot'
kernel @ 14008000 (9138040)
ramdisk @ 15000000 (2003051)
fdt @ 14f00000 (58081)
## Booting Android Image at 0x14007800 ...
Kernel load addr 0x14008000 size 8924 KiB
## Flattened Device Tree blob at 14f00000
Booting using the fdt blob at 0x14f00000
XIP Kernel Image ... OK
Using Device Tree in place at 14f00000, end 14f112e0
No PMIC found 2!

Starting kernel ...

Booting Linux on physical CPU 0x0
Linux version 4.14.98 (root@administartor) (gcc version 4.9.x 20150123 (prerelease) (GCC)) #44 SMP PREEMPT Mon Jan 27 19:20:28 IST 2020
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
OF: fdt: Machine model:  i.MX6 AOSP 9.0 Board
Memory policy: Data cache writealloc
cma: Reserved 320 MiB at 0x32000000
percpu: Embedded 18 pages/cpu @f64e7000 s41228 r8192 d24308 u73728
Built 1 zonelists, mobility grouping on. Total pages: 522290
Kernel command line: console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,fbpix=RGB32,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=128M androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=320M androidboot.selinux=permissive galcore.contiguousSize=33554432 loop.max_part=7 buildvariant=userdebug androidboot.serialno=1d2229d4ea997119 androidboot.btmacaddr=1d:22:29:d4:ea:99 androidboot.soc_type=imx6q androidboot.storage_type=emmc androidboot.boottime=1BLL:0,1BLE:5054,KL:0,KD:0,AVB:925,ODT:0,SW:0 androidboot.bootreason=watchdog androidboot.verifiedbootstate=green androidboot.slot_suffix= androidboot.vbmeta.device=PARTUUID=621ee45e-e923-4fc2-aa1d-6fd0bc488995 androidboot.vbmeta.avb_version=1.1 androidboot.vbmeta.device_state=locked androidboot.vbmeta.hash_alg=sha256 androidboot.vbmeta.size=2944 androidboot.vbmeta.digest=999aac0a122a2b1bed2062a477c07a76e66b4e5230ca8c80a4f6e3558d9127c6 androidboot.veritymode=enforcing androidboot.dtbo
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 1726220K/2097152K available (12288K kernel code, 881K rwdata, 3556K rodata, 2048K init, 531K bss, 43252K reserved, 327680K cma-reserved, 1187840K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xf8000000 - 0xff800000 ( 120 MB)
lowmem : 0xc0000000 - 0xf7800000 ( 888 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.text : 0xc0008000 - 0xc0d00000 (13280 kB)
.init : 0xc1200000 - 0xc1400000 (2048 kB)
.data : 0xc1400000 - 0xc14dc6c0 ( 882 kB)
.bss : 0xc14dc6c0 - 0xc1561448 ( 532 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
ftrace: allocating 38831 entries in 114 pages
Preemptible hierarchical RCU implementation.
Tasks RCU enabled.
NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
L2C-310 errata 752271 769419 enabled
L2C-310 enabling early BRESP for Cortex-A9
L2C-310 full line of zeros enabled for Cortex-A9
L2C-310 ID prefetch enabled, offset 16 lines
L2C-310 dynamic clock gating enabled, standby mode enabled
L2C-310 cache controller enabled, 16 ways, 1024 kB
L2C-310: CACHE_ID 0x410000c7, AUX_CTRL 0x76470001
Switching to timer-based delay loop, resolution 333ns
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Security Framework initialized
SELinux: Initializing.
Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
CPU: Testing write buffer coherency: ok
CPU0: Spectre v2: using BPIALL workaround
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x10100000 - 0x10100060
Hierarchical SRCU implementation.
smp: Bringing up secondary CPUs ...
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
CPU1: Spectre v2: using BPIALL workaround
CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
CPU2: Spectre v2: using BPIALL workaround
CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
CPU3: Spectre v2: using BPIALL workaround
smp: Brought up 1 node, 4 CPUs
SMP: Total of 4 processors activated (24.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
CPU3: update max cpu_capacity 1024
devtmpfs: initialized
CPU2: update max cpu_capacity 1024
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
futex hash table entries: 1024 (order: 4, 65536 bytes)
pinctrl core: initialized pinctrl subsystem
random: get_random_u32 called from bucket_table_alloc+0xfc/0x24c with crng_init=0
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor menu
CPU identified as i.MX6Q, silicon rev 1.5
vdd1p1: supplied by regulator-dummy
anatop_regulator_probe reg=21077
vdd3p0: supplied by regulator-dummy
vdd2p5: supplied by regulator-dummy
vddarm: supplied by regulator-dummy
vddpu: supplied by regulator-dummy
vddsoc: supplied by regulator-dummy

hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
usb_phy_generic 2000000.aips-bus:usbphy_nop1: 2000000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator
usb_phy_generic 2000000.aips-bus:usbphy_nop2: 2000000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator
i2c_imx_init_recovery_info: using scl-gpio 155 and sda-gpio 154 for recovery
i2c i2c-0: IMX I2C adapter registered
i2c i2c-0: can't use DMA, using PIO instead.
i2c_imx_init_recovery_info: using scl-gpio 108 and sda-gpio 109 for recovery
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA, using PIO instead.
i2c_imx_init_recovery_info: using scl-gpio 3 and sda-gpio 203 for recovery
i2c i2c-2: IMX I2C adapter registered
i2c i2c-2: can't use DMA, using PIO instead.
Linux video capture interface: v2.00
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
Advanced Linux Sound Architecture Driver Initialized.
Bluetooth: Core ver 2.22
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
clocksource: Switched to clocksource mxc_timer1
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 3, 32768 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 1960K
hw perfevents: no interrupt-affinity property for /soc/pmu, guessing.
hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
Bus freq driver module loaded
audit: initializing netlink subsys (disabled)
audit: type=2000 audit(0.760:1): state=initialized audit_enabled=0 res=1
workingset: timestamp_bits=14 max_order=19 bucket_order=5
Registering sdcardfs 0.1
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.26)
bounce: pool size: 64 pages
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
io scheduler mq-deadline registered
io scheduler kyber registered
pwm-backlight pwm-backlight: pwm-backlight supply power not found, using dummy regulator
ldb_init: LDB_INIT
mxc_sdc_fb fb@0: registered mxc display driver ldb
ldb_setup: LDB_SETUP
ldb_disable: LDB_DISABLE
ldb 2000000.aips-bus:ldb: Clock OFF
imx-ipuv3 2800000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
backlight: fb_notifier_callback(62): ignore first event 9.
ldb_setup: ldb setuped
Console: switching to colour frame buffer device 128x37
mxc_sdc_fb fb@1: Can't get fb option for mxcfb1!
mxc_sdc_fb fb@2: Can't get fb option for mxcfb2!
mxc_sdc_fb fb@3: Can't get fb option for mxcfb3!
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: Falling back to user helper
mxs-dma 110000.dma-apbh: initialized
imx-pgc-pd imx-pgc-power-domain.0: Linked as a consumer to 20dc000.gpc
imx-pgc-pd imx-pgc-power-domain.1: Linked as a consumer to 20dc000.gpc
i2c_imx_xfer(3) : -6
pfuze100-regulator 1-0008: unrecognized pfuze chip ID!
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 26, base_baud = 5000000) is a IMX
console [ttymxc0] enabled
21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 76, base_baud = 5000000) is a IMX
[drm] Initialized vivante 1.0.0 20120216 for platform:Vivante GCCore on minor 0
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
zram: Added device: zram0
libphy: Fixed MDIO Bus: probed
tun: Universal TUN/TAP device driver, 1.6
CAN device driver interface
PPP generic driver version 2.4.2
PPP BSD Compression module registered
PPP Deflate Compression module registered
PPP MPPE Compression module registered
pegasus: v0.9.3 (2013/04/25), Pegasus/Pegasus II USB Ethernet driver
usbcore: registered new interface driver pegasus
usbcore: registered new interface driver rtl8150
usbcore: registered new interface driver r8152
usbcore: registered new interface driver asix
usbcore: registered new interface driver ax88179_178a
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver cdc_eem
usbcore: registered new interface driver net1080
usbcore: registered new interface driver cdc_subset
usbcore: registered new interface driver zaurus
usbcore: registered new interface driver cdc_ncm
enumeration_check_probe:
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
ehci-mxc: Freescale On-Chip EHCI Host driver init_gpio
usbcore: registered new interface driver cdc_acm
cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usbserial
usbcore: registered new interface driver usbserial_generic
usbserial: USB Serial support registered for generic
usbcore: registered new interface driver ftdi_sio
usbserial: USB Serial support registered for FTDI USB Serial Device
usbcore: registered new interface driver option
usbserial: USB Serial support registered for GSM modem (1-port)
usbcore: registered new interface driver usb_ehset_test
usbmisc_imx 2184800.usbmisc: 2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
imx_usb 2184000.usb: 2184000.usb supply vbus not found, using dummy regulator
udc: set g_ci=0xe0494010
imx_usb 2184200.usb: 2184200.usb supply vbus not found, using dummy regulator
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: EHCI Host Controller
usb usb1: Manufacturer: Linux 4.14.98 ehci_hcd
usb usb1: SerialNumber: ci_hdrc.1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
usb_set_configuration enumeration_state is NULL
mfppanel_kp_init start
mfppanel_kp_probe start
input: keypad as /devices/virtual/input/input0
kp_probe end
usbcore: registered new interface driver usb_acecad
usbcore: registered new interface driver aiptek
usbcore: registered new interface driver gtco
usbcore: registered new interface driver hanwang
usbcore: registered new interface driver kbtab
ROHM BU21049 rohm_ts_init
ROHM BU21049 rohm_ts_probe!!
do_calibration start
Rohm_ts_probe: --------------------setting ready
input: Rohm-RTP-BU21049GUL as /devices/virtual/input/input1
Request IRQ Failed==>ret : 0
==>:Touchscreen Up Rohm-RTP-BU21049GUL in interrupt mode
snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-rtc-lp as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x/sz) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR SANYO protocol handler initialized
IR Sharp protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR XMP protocol handler initialized
mxc_v4l2_output v4l2_out: V4L2 device registered as video16
mxc_v4l2_output v4l2_out: V4L2 device registered as video17
usbcore: registered new interface driver uvcvideo
USB Video Class driver (1.1.1)

i2c_imx_xfer(3) : -6
mma8x5x 0-001c: read chip ID 0xfffffffa is not equal to 0x1a,0x2a,0x3a,0x4a,0x5a!
mma8x5x: probe of 0-001c failed with error -22
imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
imx2-wdt 20c0000.wdog: timeout 60 sec (nowayout=0)
device-mapper: uevent: version 1.0.3
device-mapper: ioctl: 4.37.0-ioctl (2017-09-20) initialised: [email protected]
Bluetooth: HCI UART driver ver 2.3
Bluetooth: HCI UART protocol H4 registered
Bluetooth: HCI UART protocol BCSP registered
Bluetooth: HCI UART protocol ATH3K registered
bt power gpio is:93
rfkill: BT RF going to : on
mxc_bt_rfkill_reset
mxc_bt_rfkill driver success loaded
usbcore: registered new interface driver btusb
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO
mmc0: LED_USE_HOST_NAME[mmc1] cmp[-1]
usb 1-1: new high-speed USB device number 2 using ci_hdrc
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
sdhci-esdhc-imx 2194000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2194000.usdhc: Got WP GPIO
mmc1: LED_USE_HOST_NAME[mmc1] cmp[0]
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
[DEBUG]mmc2: WLAN_USE_HOST_NAME[mmc2] cmp[0]
mmc2 bounce up to 128 segments into one, max segment size 65536 bytes
mmc2: LED_USE_HOST_NAME[mmc1] cmp[1]
mmc1: new high speed SDHC card at address aaaa
mmcblk1: mmc1:aaaa SC16G 14.8 GiB
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using DMA
mmc3: LED_USE_HOST_NAME[mmc1] cmp[1]
usb 1-1: New USB device found, idVendor=045b, idProduct=022b
usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
hub 1-1:1.0: USB hub found
hub 1-1:1.0: 3 ports detected
usb_set_configuration bmAttributes[000000E0/000000E0] status[00000001]
usb_set_configuration parent hub is self power
mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
mxc_vpu 2040000.vpu_fsl: VPU initialized
imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_KEY_ROW2 already requested by 20e0000.iomuxc; cannot claim for soc:hdmi_cec@00120000
imx6q-pinctrl 20e0000.iomuxc: pin-131 (soc:hdmi_cec@00120000) status -22
imx6q-pinctrl 20e0000.iomuxc: could not request pin 131 (MX6Q_PAD_KEY_ROW2) from group hdmicecgrp on device 20e0000.iomuxc
mxc_hdmi_cec soc:hdmi_cec@00120000: Error applying setting, reverse things back
mxc_hdmi_cec: probe of soc:hdmi_cec@00120000 failed with error -22
Galcore version 6.2.4.190076
random: fast init done
mmc[mmc3] EXT CSD REVISION[8]
mmc3: new DDR MMC card at address 0001
mmcblk3: mmc3:0001 HAG4a2 7.34 GiB
mmcblk3boot0: mmc3:0001 HAG4a2 partition 1 8.00 MiB
mmcblk3boot1: mmc3:0001 HAG4a2 partition 2 8.00 MiB
mmcblk3rpmb: mmc3:0001 HAG4a2 partition 3 4.00 MiB
[drm] Initialized vivante 1.0.0 20170808 for 130000.gpu on minor 1
caam 2100000.caam: ERA source: CAAMVID.
caam 2100000.caam: AXI pipeline throttling enabled.
caam 2100000.caam: device ID = 0x0a16010000000000 (Era 4)
caam 2100000.caam: job rings = 2, qi = 0, dpaa2 = no
caam algorithms registered in /proc/crypto
caam_jr 2101000.jr0: registering rng-caam
hidraw: raw HID events driver (C) Jiri Kosina
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
ashmem: initialized
update_probe:
info_probe:
usbcore: registered new interface driver snd-usb-audio
fsl-ssi-dai 202c000.ssi: No cache defaults, reading back from HW
Read PDN pin from device tree
imx-ak4637 sound: ak4637-aif <-> 202c000.ssi mapping ok
imx-ak4637 sound: snd-soc-dummy-dai <-> 2034000.asrc mapping ok
imx-ak4637 sound: ak4637-aif <-> 202c000.ssi mapping ok
NET: Registered protocol family 26
u32 classifier
Actions configured
Netfilter messages via NETLINK v0.30.
nf_conntrack version 0.5.0 (16384 buckets, 65536 max)
ctnetlink v0.93: registering with nfnetlink.
xt_time: kernel timezone is -0000
IPv4 over IPsec tunneling driver
ip_tables: (C) 2000-2006 Netfilter Core Team
arp_tables: arp_tables: (C) 2002 David S. Miller
Initializing XFRM netlink socket
NET: Registered protocol family 10
Segment Routing with IPv6
mip6: Mobile IPv6
ip6_tables: (C) 2000-2006 Netfilter Core Team
sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
NET: Registered protocol family 17
NET: Registered protocol family 15
can: controller area network core (rev 20170425 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20170425)
can: broadcast manager protocol (rev 20170425 t)
can: netlink gateway (rev 20170425) max_hops=1
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: BNEP socket layer initialized
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
Bluetooth: HIDP socket layer initialized
8021q: 802.1Q VLAN Support v1.8
lib80211: common routines for IEEE802.11 drivers
registered taskstats version 1
(NULL device *): hwmon_device_register() is deprecated. Please convert the driver to use hwmon_device_register_with_info().
Hot alarm is canceled. GPU3D clock will return to 64/64
imx_thermal 2000000.aips-bus:tempmon: Extended Commercial CPU temperature grade - max:105C critical:105C passive:95C
snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:14:12 UTC (852)
usb_otg_vbus: disabling
usb_h1_vbus: disabling
mipi_dsi_pwr_on: disabling
wlreg_on: disabling
ALSA device list:
#0: ak4637-audio
Freeing unused kernel memory: 2048K
init: init first stage started!
init: Using Android DT directory /proc/device-tree/firmware/android/
init: [libfs_mgr]fs_mgr_read_fstab_default(): failed to find device default fstab
init: bool android::init::FirstStageMount::InitRequiredDevices(): partition(s) not found in /sys, waiting for their uevent(s): boot, system, vbmeta, vendor
init: Wait for partitions returned after 10001ms
init: bool android::init::FirstStageMount::InitRequiredDevices(): partition(s) not found after polling timeout: boot, system, vbmeta, vendor
init: Failed to mount required partitions early ...
init: Reboot start, reason: reboot, rebootTarget: bootloader
init: Reboot ending, jumping to kernel
imx-sdma 20ec000.sdma: external firmware not found, using ROM firmware
ci_hdrc ci_hdrc.1: remove, state 1
usb usb1: USB disconnect, device number 1
usb 1-1: USB disconnect, device number 2
ci_hdrc ci_hdrc.1: USB bus 1 deregistered
reboot: Restarting system with command 'bootloader'

====================================================================

Please suggest solution if you also faced similar problem.

Thanks,

Thanaraj.

Regards,
Thanaraj Subramani
ラベル(5)
0 件の賞賛
返信
13 返答(返信)

10,792件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Which Android release are you using?

Best regards,

Diego.

0 件の賞賛
返信

10,792件の閲覧回数
ThanarajS
Contributor III

Hi Diego,

Any inputs will be helpful to solve this issue. Still we are facing the same issue.

Thanks,

Thanaraj. 

Regards,
Thanaraj Subramani
0 件の賞賛
返信

10,792件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

I apologize for the delay.

Have you used UUU to download the Android image into the board? If yes could you please tell me the command that you used? Furthermore, if you are using an eMMC or an SD card. In the case of using an SD card. Which is the size of the SD card that you are using?

Best regards,

Diego.

0 件の賞賛
返信

10,792件の閲覧回数
ThanarajS
Contributor III

Hi Diego,

Thanks for response.

Unfortunately, we are not able to use UUU tools for eMMC flash. 

We were able to boot using SD Card (8GB/16GB). The same image, we used for eMMC flash via SD Boot using fsl-sdcard-partition.sh (with minimal changes e.g: /dev/mmcblk3 and part num's). Then we observed the "FirstStageMount" issue.

FYI, We kept all required images and scripts in userdata partition for eMMC flash. eMMC Size is 8 GB

Any inputs will be helpful to solve this issue.

Regards,

Thanaraj.

Regards,
Thanaraj Subramani
0 件の賞賛
返信

10,792件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Are you telling me that you are not able to use the UUU tool for the eMMC card?

Try with the following UUU comand.

uuu_imx_android_flash.bat -f imx6qp -p sabresd -e

Whit that command. It should work. The problem probably is because the partitio_table.img is the incorrect one.

Hope this may help you.

Best regards,

Diego.

0 件の賞賛
返信

10,792件の閲覧回数
ThanarajS
Contributor III

Hi Diego,

Thanks for response.

Yes. We don't have USB support to use UUU tool. Only the way we can flash via SD Boot to eMMC card.

if partition_table.img is incorrect, how its working for SD card boot?

 

Regards,

Thanaraj.

Regards,
Thanaraj Subramani
0 件の賞賛
返信

10,792件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

This is because the partition table depends on the size of the storage that you are going to use.

If your current storage does not fit with your partition table. You will get errors at the time you are mounting the partitions.

How are you copying and partitioning the eMMC memory?

Best regards,

Diego.

0 件の賞賛
返信

10,792件の閲覧回数
ThanarajS
Contributor III

Hi Diego,

We are using partition-table.img (for 8GB) for SD Card and eMMC memory partition.

How are you copying and partitioning the eMMC memory?

First we are flashing SD card (normal way), then we are copying all the required (for eMMC) files and images and scripts to userdata partition by mounting. then we are booting board via SD boot, after boot we are running modified fsl-sdcard-partition.sh script in board shell prompt to flash into mmcblk3 (eMMC).

Regards,

Thanaraj.

 

Regards,
Thanaraj Subramani
0 件の賞賛
返信

10,792件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we cannot support this. Since the only tool that we have to download the image into the eMMC is UUU. What we do recommend is to use that tool. I apologize for the inconvenience this may give you.

Best regards,

Diego.

0 件の賞賛
返信

10,792件の閲覧回数
krishnandu_bisw
Contributor II

Hello,

I am also the facing same issue. I've tried both ways of flashing, the output is same.

Do you know the any other way, which might help in debugging the cause? So that we could fix it in the source code.

Regards,

Krishnandu

0 件の賞賛
返信

10,792件の閲覧回数
chenguoyin
NXP Employee
NXP Employee

1. if boot from emmc, please remove your sdcard from the board firstly to see whether it helps.

2. check the dts to config the dev_xxx with the storage node you are using.

/ {
firmware {
android {
fstab {
/delete-node/ system;
vendor {

0 件の賞賛
返信

10,792件の閲覧回数
krishnandu_bisw
Contributor II

1. I'm using SD card for booting.

2. dts configuration for dev_sd is to correct node is:

fstab{ 

     system{

            compatible = "android,system";

            dev_sd = "/dev/block/platform/soc0/soc/2100000.aips-bus/2198000.usdhc/by-name/system";   //SD3

            dev_emmc = "/dev/block/platform/soc0/soc/2100000.aips-bus/219c000.usdhc/by-name/system";   //SD4

            type = "ext4";
            mnt_flags = "ro,barrier=1,inode_readahead_blks=8";
            fsmgr_flags = "wait,avb";

      }

      vendor{

            compatible = "android,vendor";  

            dev_sd = "/dev/block/platform/soc0/soc/2100000.aips-bus/2198000.usdhc/by-name/vendor";
            dev_emmc = "/dev/block/platform/soc0/soc/2100000.aips-bus/219c000.usdhc/by-name/vendor";

            type = "ext4";
            mnt_flags = "ro,barrier=1,inode_readahead_blks=8";
            fsmgr_flags = "wait,avb";

      }

}

0 件の賞賛
返信

10,792件の閲覧回数
ThanarajS
Contributor III

Hi Diego,

I referred the "AndroidTM User's Guide, Rev. P9.0.0_2.2.0-ga, 08/2019" doc and used "imx-p9.0.0_2.2.0-ga.tar.gz" release.

 

Best regards,

Thanaraj.

Regards,
Thanaraj Subramani
0 件の賞賛
返信