Filling zeros in frame buffer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Filling zeros in frame buffer

2,065件の閲覧回数
titusstalin
Contributor V

Dear All,

1)

How can I fill the zeros in frame buffer ?

Actually I'm getting some alignment issues in camera frame buffer, then I found that the alignment issue occurs if camera send lesser data than what I've requested.

Say for ex, I'm requesting 1478656bytes of data and if camera sends 1440000bytes of data, there issues comes.

So what I think, can we fill zeros for the rest of the space ?

Thanks for your support.

Regards,

Titus S.

ラベル(1)
3 返答(返信)

1,929件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello

  I am afraid, no way to fill the rest of buffer by zeros in IPU. Application should

know frame size or clear buffers before using in software.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,929件の閲覧回数
titusstalin
Contributor V

Thanks Yuri for your support.

0 件の賞賛
返信

1,929件の閲覧回数
titusstalin
Contributor V

Any support on this post ?

0 件の賞賛
返信