Filling zeros in frame buffer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Filling zeros in frame buffer

2,055 Views
titusstalin
Contributor V

Dear All,

1)

How can I fill the zeros in frame buffer ?

Actually I'm getting some alignment issues in camera frame buffer, then I found that the alignment issue occurs if camera send lesser data than what I've requested.

Say for ex, I'm requesting 1478656bytes of data and if camera sends 1440000bytes of data, there issues comes.

So what I think, can we fill zeros for the rest of the space ?

Thanks for your support.

Regards,

Titus S.

Labels (1)
3 Replies

1,919 Views
Yuri
NXP Employee
NXP Employee

Hello

  I am afraid, no way to fill the rest of buffer by zeros in IPU. Application should

know frame size or clear buffers before using in software.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,919 Views
titusstalin
Contributor V

Thanks Yuri for your support.

0 Kudos
Reply

1,919 Views
titusstalin
Contributor V

Any support on this post ?

0 Kudos
Reply