Hello,
We have successfully built Android 11 for the iMX8 but receive the following errors when attempting to build the SDK using the command "make sdk". The complete build log is attached.
development/build/sdk-linux-x86.atree:34: couldn't locate source file: lib64/libclang_android.so
development/build/sdk-linux-x86.atree:36: couldn't locate source file: lib64/libaapt2_jni.so
development/build/sdk.atree:53: couldn't locate source file: bin/dmtracedump
development/build/sdk.atree:54: couldn't locate source file: bin/etc1tool
development/build/sdk.atree:80: couldn't locate source file: bin/aapt
development/build/sdk.atree:81: couldn't locate source file: bin/aapt2
development/build/sdk.atree:82: couldn't locate source file: bin/aidl
development/build/sdk.atree:83: couldn't locate source file: bin/split-select
development/build/sdk.atree:84: couldn't locate source file: bin/zipalign
development/build/sdk.atree:87: couldn't locate source file: bin/llvm-rs-cc
development/build/sdk.atree:88: couldn't locate source file: bin/bcc_compat
development/build/sdk.atree:133: couldn't locate source file: bin/apksigner
development/build/sdk.atree:134: couldn't locate source file: framework/apksigner.jar
development/build/sdk.atree:137: couldn't locate source file: bin/dx
development/build/sdk.atree:138: couldn't locate source file: framework/dx.jar
development/build/sdk.atree:237: couldn't locate source file: system-qemu.img
development/build/sdk.atree:238: couldn't locate source file: vendor-qemu.img
development/build/sdk.atree:239: couldn't locate source file: ramdisk-qemu.img
development/build/sdk.atree:241: couldn't locate source file: data/misc
development/build/sdk.atree:243: couldn't locate source file: VerifiedBootParams.textproto
ninja: build stopped: subcommand failed.
20:51:00 ninja failed with: exit status 1
#### failed to build some targets (01:02 (mm:ss)) ####
We would appreciate any help in this matter.
Thanks,
Tom
Hi
Did you source the env and lunch before make?
BR
Zhiming
Hello Zhiming,
Sorry for the delay in my response. Yes, I ran the following commands...
source build/envsetup.sh
lunch mek_8q-userdebug
Then I attempted to build sdk using the commands both the same results...
make sdk
make win_sdk
Thanks,
Tom
Hi tombo1
Can you try to lunch eng mode?
BR
Zhiming
Hello Zhiming,
I rebuilt the environment and achieved the same errors from my original post. The commands I used for this attempt...
lunch mek_8q-eng
./imx-make.sh -j16 2>&1 | tee build-log.txt
#### build completed successfully (02:08:17 (hh:mm:ss)) ####
make sdk
Received same error as original post
Thanks for your continued help,
Tom
I think the full steps are:
1. Do the standard build
lunch mek_8q-eng
make
2. Build the missing tools
make dmtracedump
make etc1tool
make split-select
make bcc_compat
make apksigner
make dxmake libaapt2_jni
make layoutlib-legacy
3. a) Edit the file development/build/sdk.atree to comment out the reference to userdata.img
##############################################################################
# System image Component
##############################################################################
# System images + Kernel
system.img system-images/${PLATFORM_NAME}/${TARGET_CPU_ABI}/system.img
ramdisk.img system-images/${PLATFORM_NAME}/${TARGET_CPU_ABI}/ramdisk.img
#userdata.img system-images/${PLATFORM_NAME}/${TARGET_CPU_ABI}/userdata.img
system/build.prop system-images/${PLATFORM_NAME}/${TARGET_CPU_ABI}/build.prop
# Note: the kernel image is handled by sdk-android-<abi>.atree now.
3. b) Alternatively, it appears that you can enable the creation of userdata.img (I have not tried this): https://community.nxp.com/docs/DOC-105198
4. Edit the file development/build/sdk.atree (again) to comment out the reference to EmulatorSmokeTests.apk
##############################################################################
# Tests Component
##############################################################################
#system/app/EmulatorSmokeTests/EmulatorSmokeTests.apk tests/emulator-test-apps/EmulatorSmokeTests.apk
5. Build the sdk
make sdk
Hello,
Thanks for your response. I attempted to follow these steps but...
There are no build rules for layoutlib-legacy
and there is no mention of EmulatorSmokeTests.apk in the sdk.atree file.
Are you sure these build rules will work for building imx-automotive-11.0.0_1.1.0 SDK?
Your continued help in this matter would be appreciated.
Thanks,
Tom
PS I believe I saw these build suggestions in a nearly three year old post from July of 2018 as well. I did attempt them previously.
Is anyone able to build the SDK?
Hi
I have fixed this issue
make dmtracedump -j8
make etc1tool -j8
make libaapt2_jni -j8
make aapt -j8
make aapt2 -j8
make aidl -j8
make split-select -j8
make zipalign -j8
make llvm-rs-cc -j8
make bcc_compat -j8
make apksigner -j8
make dx -j8
Then comment codes in /android_build/development/build/sdk.tree
# System images + Kernel
#system-qemu.img system-images/${PLATFORM_NAME}/${TARGET_CPU_ABI}/system.img
#vendor-qemu.img system-images/${PLATFORM_NAME}/${TARGET_CPU_ABI}/vendor.img
#ramdisk-qemu.img system-images/${PLATFORM_NAME}/${TARGET_CPU_ABI}/ramdisk.img
device/generic/goldfish/data/etc/userdata.img system-images/${PLATFORM_NAME}/${TARGET_CPU_ABI}/userdata.img
#data/misc system-images/${PLATFORM_NAME}/${TARGET_CPU_ABI}/data/misc
system/build.prop system-images/${PLATFORM_NAME}/${TARGET_CPU_ABI}/build.prop
#VerifiedBootParams.textproto system-images/${PLATFORM_NAME}/${TARGET_CPU_ABI}/VerifiedBootParams.textproto
These doesn't affect sdk.
BR
Zhiming