Failed to mount system image!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Failed to mount system image!

3,359件の閲覧回数
oliverkuo
Contributor IV

Hi,

 

  I'm trying to port Android L5.0.0-1.0.0 on our custom board, but fail to boot into system image.

From the boot log, looks like VERITY_METADATA_MAGIC_NUMBER can't be read and fail to mount mmcblk3p5.

fs_mgr: Couldn't find verity metadata at offset 0!

fs_mgr: Could not set up verified partition, skipping!

EXT4-fs (mmcblk3p4): Ignoring removed nomblk_io_submit option

EXT4-fs (mmcblk3p4): recovery complete

EXT4-fs (mmcblk3p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic

fs_mgr: __mount(source=/dev/block/mmcblk3p4,target=/data,type=ext4)=0

EXT4-fs (mmcblk3p6): Ignoring removed nomblk_io_submit option

EXT4-fs (mmcblk3p6): recovery complete

EXT4-fs (mmcblk3p6): mounted filesystem with ordered data mode. Opts: nomblk_io_submit

fs_mgr: __mount(source=/dev/block/mmcblk3p6,target=/cache,type=ext4)=0

EXT4-fs (mmcblk3p7): mounted filesystem with ordered data mode. Opts: (null)

fs_mgr: __mount(source=/dev/block/mmcblk3p7,target=/device,type=ext4)=0

Could someone give me a hint which step or setting I missed?

What should I do to keep verified boot enabled and mount system image successfully, except "androidboot.dm_verity=disabled"?

 

Thanks,

Oliver

Original Attachment has been moved to: boot_failed.log.zip

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

2,226件の閲覧回数
jonathantaylor
Contributor II

How do you get the boot log?  I might have the same problem, but I don't know how to see that!  When you run the MfgTool, it looks like it formats everything, so I can't reboot with a valid system.img to use the device.  When it doesn't boot, how do you interact with the board to read something from it?

0 件の賞賛
返信

2,226件の閲覧回数
oliverkuo
Contributor IV

Hi,

You could download your image by modifying the script of MFGTool.

Please refer to the document of MFGTool for detail.

Best regards,

Oliver

0 件の賞賛
返信