FSL High-speed Electrical Test Mode Support in Kernel 3.10.17

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FSL High-speed Electrical Test Mode Support in Kernel 3.10.17

2,188 次查看
DipenPatel1z
Contributor III

Dear All,

I was looking for FSL High-speed Electrical Test Mode Support in kernel 3.10.17 but can not find the hset driver arc_hset.c. It seems in kernel 3.10.17 USB host driver is now based on Chip Media IP which is different than ARC based driver.

Does anyone have any idea if such driver is already available for kernel 3.10.17? We need to perform USB compliance testing for our product.

Regards,

Dipen Patel

标签 (3)
标记 (3)
0 项奖励
回复
2 回复数

1,865 次查看
satheshkumarman
Contributor II

Hi,

I'm also looking for answer for the same query?

If you get the solution already,  please share some information here.

Thanks.

Sathesh

0 项奖励
回复

1,865 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Dipen,

Have you checked the following thread, which includes many USB tests under Linux 3.10.10 BSP?

https://community.freescale.com/thread/330155


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复