FRDM-IMX8MPLUS: System resets immediately when connecting Lauterbach TRACE32.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-IMX8MPLUS: System resets immediately when connecting Lauterbach TRACE32.

Jump to solution
1,144 Views
neko
Contributor I

Hi NXP Community,

I am working with the FRDM-IMX8MPLUS development board and trying to debug it using a Lauterbach TRACE32 via the 10-pin JTAG interface.

I am encountering a severe issue: the system resets/powers off immediately the moment I plug the JTAG cable into the board while it is running.

neko_0-1780499260757.png

I try to execute SYStem.Mode Attach in the TRACE32 software, it fails and returns the error: debug port time-out at UNKNOWN.


I suspect this behavior is tied to the Cold Reset signal path. Before connecting the debugger, both VTREF (Pin 1) and JTAG_RESET (Pin 10) are stable at 1.8V. Upon plugging in the TRACE32, JTAG_RESET instantly drops to 0V, which coincides with VTREF falling to 0.7V and crashing the system (the green led turn off).

How can I properly configure the hardware/software to avoid the reset issue and successfully attach the debugger?

Thanks in advance!

0 Kudos
Reply
1 Solution
1,130 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

Could you please try connecting TRACE32 before target POR?

Regards

View solution in original post

0 Kudos
Reply
3 Replies
1,121 Views
neko
Contributor I

Hi,

I also attach images of the board when Trace32 is plugged in and when it is unplugged.

neko_0-1780510030551.png

neko_1-1780510045663.png


Regard

0 Kudos
Reply
1,123 Views
neko
Contributor I

Hi Joseph,

I am following these steps:

  1. Power off the IMX8MP board and connect Trace32.
  2. Power on the board.

However, the board does not boot. There is no output on the serial UART, and LED D16 does not turn on.

If I disconnect Trace32, the board boots successfully again.

Regards,

0 Kudos
Reply
1,131 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

Could you please try connecting TRACE32 before target POR?

Regards

0 Kudos
Reply