FIQ support for IMX6 Linux BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FIQ support for IMX6 Linux BSP

4,400件の閲覧回数
hengyewlim
Contributor III

Hi,

I am trying to get FIQ working on IMX6 SoloX. I ported the changes from https://community.nxp.com/docs/DOC-95578  and was able to trigger the FIQ in assembly. But it will crashed when calling into the "C" code FIQ handler. Do you have an updated version for the AVB demo ported to the latest Linux 4.1.15 BSP which I can refer to?

Thank

HY

ラベル(2)
0 件の賞賛
返信
1 返信

3,970件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Heng Yew Lim,

There is no newer release of the demo that it’s ported to the 4.1.15 BSP.

The most up-to date alternative would be the AVB Stack for the i.MX6. This is provided by NXP Professional Services and you can find more information on the link below. (Please keep in mind this is moderated Software)

http://www.nxp.com/products/software-and-tools/run-time-software/professional-services-software-tech...

My apologies for the inconvenience.

Regards,

0 件の賞賛
返信