Hi,
I'm working on a project where we have iMX6ULL processor and I'm trying to get Ethernet working.
My question is about FEC blocks and ENET signals.
Can I connect ENET1 signals to FEC2 controller (in Device Tree)?
Or do the FECs and ENET pinctrl always have to be connected as "fixed pairs", i.e. FEC1 must always use ENET1 pinctrl and FEC2 must always use ENET2 pinctrl?
Thanks & best regards,
Jari
Solved! Go to Solution.
Hi Jari
right, ENET1 specific signals can be found in
sect.4.1.1 Muxing Options i.MX 6ULL Applications Processor Reference Manual
Best regards
igor
Hi Jari
in theory this is possible, however seems there are only two options
ENET1_MDC signal from pad ENET2_RX_DATA1
ENET1_MDIO signal from pad ENET2_RX_DATA0
according to sect.4.1.1 Muxing Options i.MX 6ULL Applications Processor Reference Manual
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thanks for your fast response!
Couple of additional questions below.
On my HW FEC2 is disabled (corresponding Fuse is burned), so, in fact I would use FEC1.
In HW the Ethernet signals are connected to ENET2 (ENET2_TX_DATA0, ENET2_TX_DATA1 , etc.).
For MDIO bus I would use MX6UL_PAD_GPIO1_IO06__ENET1_MDIO and MX6UL_PAD_GPIO1_IO07__ENET1_MDC. Should this setup work?
Does the fact that FEC2 is disabled (fused) have any impact? Would ENET2 interface still work?
Regards,
Jari
Hi Jari
if FEC2 is disabled it will not work in any pinmux combinations.
Best regards
igor
Hi Igor,
Thanks again for your answer!
So, the only way I could get Ethernet working is to use the ENET1 specific muxing for MDIO and MDC and ENET1 specific signals for the actual Ethernet signals, am I right?
Regards,
Jari
Hi Jari
right, ENET1 specific signals can be found in
sect.4.1.1 Muxing Options i.MX 6ULL Applications Processor Reference Manual
Best regards
igor
Hi Igor,
Thanks for your support!
I have no further questions at this point. We can close this thread.
Best regards,
Jari