FEC driver problem on i.mx25

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FEC driver problem on i.mx25

3,002 Views
sethbollinger
Contributor II

Hello All,

 

Sometimes the FEC driver will stall with a descriptor in the DMA ring that's ready for transmit but FEC_X_DES_ACTIVE bit is not enabled.  This buffer will remain jammed in the ring until another transmit request is queued.

 

Has anyone else seen this issue?  Is there a known solution?

 

We have worked around the problem by keeping a count of tx ready descriptor, then we check that count at the end of fec_enet_rx().  If we have at least one tx descriptor ready, but the DMA TX controller is not active, we give it a bump.

 

We would like to avoid this situation rather than work around it.

 

Thanks,

 

Seth

Tags (1)
4 Replies

2,819 Views
wolfgang_gaerbe
Contributor I

Comment found in actual u-boot driver:

================================================================

When only one BD is in
 * use it must be marked with the WRAP bit to use it for every transmitt.
 * This bit in combination with the READY bit results into double transmit
 * of each data buffer. It seems the state machine checks READY earlier then
 * resetting it after the first transfer.
 * Using two BDs solves this issue.

========================================================

We observed similar problems on processing the last descriptor in a ringbuffer.....

What´s even more scary - is that is obvious race condition depends somehow on chip revisions.

Identical code failed on our board - but not on the evk. So be careful with the last descriptor ;-))

2,819 Views
fabio_estevam
NXP Employee
NXP Employee

I don't have any details about the problem you mention. 2.6.35 kernel does not receive any more updates, so it is a good idea to try 3.0 to check if the problem still exists or not.

 

If you see the problem, then the drivers/net folks would be interested in fixing  it.

0 Kudos
Reply

2,819 Views
sethbollinger
Contributor II

We don't have a BSP for the 3.0 kernel.  It will take some time to get that working.  I will let you know when I gather that data.

Is there a reason you think this is fixed in kernels beyond 2.6.35.14?

Thanks,

Seth

0 Kudos
Reply

2,819 Views
fabio_estevam
NXP Employee
NXP Employee

Could you please try a 3.0 kernel and let us know if you face the same issue?

 

If you do, please list the steps on how to reproduce this problem.

 

Regards,

 

Fabio Estevam

0 Kudos
Reply