External RTC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

External RTC

1,554 Views
lk22
Contributor I

HI,

We are using internal RTC with a crystal of 9pF load capacitance and two 16pF capacitors on i.MX6S processor. The clock is about 2 to 3 seconds lagging behind on every 2 days. How this can be corrected?

We are thinking to use external RTC, which will provide clock on I2C lines to processor. Will there be any issue in booting or timing on using external RTC?

with regards

Lalit

Labels (2)
0 Kudos
Reply
1 Reply

1,417 Views
art
NXP Employee
NXP Employee

Q. How this can be corrected?

A. Check the crystal tolerance first.

Q. Will there be any issue in booting or timing on using external RTC?

A. No, there should be no any issue. You just have to slightly modify the software to load the value of the external RTC to the internal one each boot time.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply