External PCIe video solution can use internal GPU ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

External PCIe video solution can use internal GPU ?

1,315 Views
weikeng-jimmy
Contributor III

Hi Sir,

I have a question:

If we are able to have an external PCIe video solution, can we use internal GPU for this external display output?

As far as I know, all display ports of imx6 are routed to internal IPUs.  When external video device create a fb device , is it like a imx6 internal fb device can use GPU 3D graphic engine?

Thanks!

Labels (2)
0 Kudos
Reply
1 Reply

1,179 Views
igorpadykov
NXP Employee
NXP Employee

Hi JIMMY

yes, one can use GPU with external PCIe video solution,

as GPU works with data located in memory buffer.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply