External PCIe video solution can use internal GPU ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

External PCIe video solution can use internal GPU ?

1,317件の閲覧回数
weikeng-jimmy
Contributor III

Hi Sir,

I have a question:

If we are able to have an external PCIe video solution, can we use internal GPU for this external display output?

As far as I know, all display ports of imx6 are routed to internal IPUs.  When external video device create a fb device , is it like a imx6 internal fb device can use GPU 3D graphic engine?

Thanks!

ラベル(2)
0 件の賞賛
返信
1 返信

1,181件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JIMMY

yes, one can use GPU with external PCIe video solution,

as GPU works with data located in memory buffer.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信