Hello,
The i.MX8QM datasheet, in Section 4.1.4 states: " The system clock input requires a crystal using the internal oscillator amplifier."
Later in footnote 4 it states: "Fundamental frequency crystal with internal oscillator amplifier."
In numerous places in this section, the document explicitly mentions crystal and external clock for RTC_XTALI, but never for XTALI.
This implies that an external clock is not supported.
But later in Section 4.5.1 is titled "XTALI and RTC_XTALI (Clock Inputs) DC Parameters" implying that external clock input is supported for XTALI.
But in that section, it talks only about VIH and VIL for RTC_XTALI and is completely silent about high speed XTALI.
Questions:
1) For applications where the system will always be running and will never go into standby or shutdown modes, can an external 24MHz oscillator, connected to XTALI pin, be used?
2) What are the voltage levels for this external clock input?
Regards,
hwasti
解決済! 解決策の投稿を見る。
Hello,
1) For applications where the system will always be running and will never go into standby or shutdown modes, can an external 24MHz oscillator, connected to XTALI pin, be used?
Yes, the chip has two XTAL modules, 24MHz XTAL and 32KHz XTAL modules (All of these modules needs to use an external clock source, you could use our MEK as reference, you can use a crystal or oscillator).
2) What are the voltage levels for this external clock input?
The 24 MHz oscillator can be driven with an external signal at the XTALI pin. The input voltage should never exceed the oscillator supply voltage (VDD_SCU_XTAL_1P8).
The 32 KHz oscillator can be driven with an external signal at the RTC_XTALI pin. The input voltage should never exceed the oscillator supply voltage (VDD_SNVS_LDO_1P8_CAP).
Here the specifications:
The processor can also accept a 1.8 V logic level clock. The specification input voltages for are the next:
VIH between (0.5 X VDD +0.5v) and VDD
VIL between 0 and (0.5 VDD - 0.5v)
Best regards.
Hi Jorge,
Your initial reply was likely referencing a different chip. Thank you for correcting it so quickly.
Regards.
Answer corrected, I apologize for the confusion.
Best regards.
Hello,
1) For applications where the system will always be running and will never go into standby or shutdown modes, can an external 24MHz oscillator, connected to XTALI pin, be used?
Yes, the chip has two XTAL modules, 24MHz XTAL and 32KHz XTAL modules (All of these modules needs to use an external clock source, you could use our MEK as reference, you can use a crystal or oscillator).
2) What are the voltage levels for this external clock input?
The 24 MHz oscillator can be driven with an external signal at the XTALI pin. The input voltage should never exceed the oscillator supply voltage (VDD_SCU_XTAL_1P8).
The 32 KHz oscillator can be driven with an external signal at the RTC_XTALI pin. The input voltage should never exceed the oscillator supply voltage (VDD_SNVS_LDO_1P8_CAP).
Here the specifications:
The processor can also accept a 1.8 V logic level clock. The specification input voltages for are the next:
VIH between (0.5 X VDD +0.5v) and VDD
VIL between 0 and (0.5 VDD - 0.5v)
Best regards.