How to connect SJ1105Q EVB into imx8qm?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to connect SJ1105Q EVB into imx8qm?

298 Views
jarinp_rd
Contributor I

Hi All,

I have a requirement to have multiple automotive ethernet ports and I have got guideline from @lukaszadrapa that we have to use SJA1105Q-EVB on i.MX 8QM board.

 

As per my understandings,

Insert MCIMX8QM-CPU card on MCIMX8-8X-BB base board using Board-to-Board Connector. Also insert SJA1105Q-EVB with base board using Sabre connector. 

 

1) is the above statement correct?

2) As SJA1105Q-EVB is an extension board for imx8QM it won't be enabled by default if we follow Linux guide from NXP. Is the following community link details sufficient for bringing up these ports in SJA1105Q-EVB?

https://community.nxp.com/t5/i-MX-Processors/The-four-phys-connected-to-sja1105Q-cannot-be-loaded-no...

 

Looking forward for your reply on the same.

 

Thanks & Regards,

Jarin P

0 Kudos
Reply
1 Reply

266 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

Yes, but it was included until the revision 5.15.71kernel, so please take in mind this consideration.

Regards

0 Kudos
Reply