EdgeLock_SetClock(kCLOCK_EDGELOCK_ClockRoot_MuxOscRc400M, 2); Crashs my debug whenever it is called in an example project. I'm using this sdk com.nxp.mcuxpresso.sdk.sdk_2.x_mimxrt1180-evk_p2site_2.16.100.2019112514465377118357287039883
解決済! 解決策の投稿を見る。
Hi @jett ,
Thank you for your updated information.
Hi Jett, your chip is PIMXRT1189CVMBA, means Silicon Rev is A0.
I consulted an RT1180 series expert, His response was "The RT1180 A0 chip cannot use the latest SDK library, and the latest SDK library can be used by the RT1170 B0 ".
Wish it helps you.
If you still have question about it, please kindly let me know.
Wish you a nice day!
mayliu
Mayliu,
I'm using the default jumper configuration, I'm following the guidance from those documents. I'm using the MIMXRT1180-EVK board with the following tags on the back; SCH-50577 REV B and 700-50577 REV x5. The SDK version is 2.16, MCUXpresso IDE is 24.9.25. I was using the evkmimxrt1180_rgpio_led_output_cm33 project but I have tried around 10 example projects and they all work only if I comment out the EdgeLock_SetClock function. I have tried the evkmimxrt1180_rgpio_led_output_cm7 project. I'm using the LinkServer MCU-Link USB.
I have attached my setup as well as where I break point at and what error I get after I hit continue
Hi @jett ,
Thank you for your updated information.
Hi Jett, Please take a picture of the silk screen on the chip of the NXP1180. It would be better if you print it out.
Best Regards
mayliu
I have attached a photo and it is written down below
PIMXRT1189CVMBA
0P96D
CTZA2221D
I did a little more digging.
The kCLOCK_RootEdgelook div is 3 and kCLOCK_RootEdgelook mux is 1 on boot
Inside of ELE_BaseAPI_ClockChangeStart
S3MU_SendMessage comes back as successful however
the response from ele_mu_get_response_baseapi contains 0xf429 at rmsg[1] instead of 0xd6 (RESPONSE_SUCCESS).
Hi @jett ,
Thank you for your updated information.
Hi Jett, your chip is PIMXRT1189CVMBA, means Silicon Rev is A0.
I consulted an RT1180 series expert, His response was "The RT1180 A0 chip cannot use the latest SDK library, and the latest SDK library can be used by the RT1170 B0 ".
Wish it helps you.
If you still have question about it, please kindly let me know.
Wish you a nice day!
mayliu
Hi @jett ,
Dear Jett, if your question is solved, please tell me to close this case, thanks.
Wish you a nice day!
Best Regards
mayliu
Hi @jett ,
Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.
I import SDK demo "evkmimxrt1180_rgpio_led_output_cm7", using MIMXRT1180-EVK board, SDK version is 2.16, MXUXPresso IDE is 24.9.25. I download the program, EdgeLock_SetClock function was called, and project works normal, So please check next points:
1: Please check your board Boot mode setting and other board setting.
I suggest you can refer the following link .
https://www.nxp.com/webapp/Download?colCode=UM12021
2:Please make sure your Board , MCUXPresso IDE , SDK is matched.
In the SDK demo, readme.md file describe more detail information.
For more information, maybe you can refer the next link:
https://www.nxp.com/docs/en/quick-reference-guide/IMXRT1180QSG.pdf
Wish it helps you.
If you still have question about it, please kindly let me know.
Best Regards
mayliu