Ethernet is not working in U-Boot for imx6ul

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Ethernet is not working in U-Boot for imx6ul

1,004 次查看
obulesu_veggidi
Contributor II

Hi All,

i am facing issue in u-boot, while trying to ping/dhcp any network related commands, my board(imx6ul) is getting reset by u-boot.

Please find bellow logs, help me if any one have solution for this. Thanks in advance.

 

U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+ga57b13b (Mar 01 2021 - 12:57:35 +0530)

CPU: Freescale i.MX6UL rev1.2 528 MHz (running at 396 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 34C
Reset cause: POR
Board: MX6UL 14x14 EVK
I2C: ready
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Display: TFT43AB (480x272)
Video: 480x272x24
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc0 is current device
Net: FEC1
Normal Boot
Hit any key to stop autoboot: 0
=> <INTERRUPT>
=> <INTERRUPT>
=> dhcp
BOOTP broadcast 1
data abort
pc : [<9ff82584>] lr : [<9ff83d8c>]
reloc pc : [<87839584>] lr : [<8783ad8c>]
sp : 9ef46cb8 ip : 00000089 fp : 9ff539b8
r10: 00000001 r9 : 9ef46eb8 r8 : 9ffec768
r7 : 0000000e r6 : 9ffeeab0 r5 : 00000000 r4 : 9ffecc4e
r3 : 00060101 r2 : 00000008 r1 : 9ffecc22 r0 : 0000000e
Flags: nZCv IRQs off FIQs off Mode SVC_32
Resetting CPU ...

resetting ...

 

0 项奖励
回复
1 回复

994 次查看
joanxie
NXP TechSupport
NXP TechSupport

you must use 4.1.15? this is very old bsp version, and we don't update this version, do you mind upgrading your bsp to the latest version? if still have issue, let me reproduce this

0 项奖励
回复