Ethernet failure issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet failure issue

2,073件の閲覧回数
vineethhegde
Contributor II

I am testing a board based on i.MX6Q processor. in that ethernet ping test is failed. The component mounting is done as per the  schematics. And every voltage , clock frequency are proper. Please suggest the solution.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,907件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi vineeth113

first check 125MHz clock, it should be outputed from ethernet phy and should have

correct duty cycle, if not, then you have to use a 125MHz oscillator for both i.MX6

and phy, the tolerance is +/-50ppm. Please check timings described in sect.4.11.5.3

RGMII Signal Switching Specifications IMX6DQCEC with oscilloscope

ENET_REF_CLK (ball V22) duty-cycle requirements on i.MX6

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,907件の閲覧回数
vineethhegde
Contributor II

in that same board Ethernet phy IC is replaced then also issue persist.

0 件の賞賛
返信

1,907件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

measure Ethernet phy timings using oscilloscope and

check with datasheet requirements

0 件の賞賛
返信