Ethernet Registers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet Registers

2,119 Views
saida
Contributor II

Ethernet Registers:

Hi I.mx6 community

Ethernet Registers are not accessible in my i.mx6 dual lite processor

how to enable these registers

thanks in advance

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

1,987 Views
jimmychan
NXP TechSupport
NXP TechSupport

what bsp are you using?

0 Kudos
Reply

1,987 Views
saida
Contributor II

hi

its working, i am working on lwip stack implementation

1. MAC address is stored in FUSE MAP registers at address of registers are 0x021bc620 and 630 but when i am reading through DS5 debugger and in u-boot its showing zero only, even if MAC_LOCK is 0.

how can i find MAC of my i.mx6 duallite core ?

2. i am trying to run http server example application from IMX6SDK with Static IP option but its not running when i trying to access a web page

3. can any one give the solution to my problem or any ref doc.

4. you can send working code of httpserver so that i will try it

5. how can i achieve full implementation lwip stack for all applications

thank you and regards

saida

0 Kudos
Reply

1,987 Views
qinghuazhu
Contributor III

Can you describe the detail. How do you access the register and what the error is.

0 Kudos
Reply