Ethernet Download speed is slow.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet Download speed is slow.

1,464件の閲覧回数
lifusong
Contributor IV

Dear sir.

Ethernet Download file speed is slow.how to fix this issue.

100M/1000M has the same speed,4MB/s

through web server download file.

android 5.0.2 kernel 3.10.53 u-boot 2014.04

and body can help me?

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

1,316件の閲覧回数
art
NXP Employee
NXP Employee

This is not a known issue. Most likeky this is the problem witn network connection on your side. Please check with your service provider.


Have a great day,
Artur

0 件の賞賛
返信

1,316件の閲覧回数
lifusong
Contributor IV

Dear Artur.

   I tested on the demo board.

our router support 1G link speed. and computer and demo board link with one router.

and if use others computer download the file through web server ,the speed is very fast.

only demo board speed is slow.

0 件の賞賛
返信

1,316件の閲覧回数
lifusong
Contributor IV

And the office demo image burn to demo board has this issue.

0 件の賞賛
返信