Error opening /dev/fb0: No such file or directory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error opening /dev/fb0: No such file or directory

3,341 Views
warrenharper
Contributor I

   I have been trying to build core-image-full-cmdline with the latest kernel but I cannot seem to get it to work. The board boots up but nothing is displayed on the screen. In the boot log I am seeing:

Error opening /dev/fb0: No such file or directory

 

   I assume that the driver is not being loaded correctly. I am pulling https://github.com/Freescale/linux-fslc - (branch 4.8.x +fslc) in my recipe. The patch I am applying to the repo is attached. I believe the problem lies in the fact the correct driver is not being loaded. I believe the files in question are the dts files. 

 

The board I am using uses a SMARC card. This is the name of the board SMA-IMX6QI-DVY.

 

I have attached:

  • 0001-SMARC-revisions.patch - the patch i am applying to the repo

  • bootlog.txt - the bootlog

 

Thanks, 

 

Warren

Original Attachment has been moved to: bootlog.txt.zip

Original Attachment has been moved to: 0001-SMARC-revisions.patch.zip

0 Kudos
Reply
1 Reply

2,561 Views
igorpadykov
NXP Employee
NXP Employee

Hi Warren

this may be posted on meta-fsl-arm mailing list, so that someone familiar with

that board could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale

Latest nxp official bsp is L4.1.15 with documentation located on

i.MX 6 Series Software and Development Tool|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply