Error in documentation IMX6DQ6SDLSRM.pdf

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error in documentation IMX6DQ6SDLSRM.pdf

2,058 Views
frédéric
Contributor III

In the IMX6DQ6SDLSRM.pdf file (mine is 8423886 bytes), page 570 Figure B-112, bits 15 to 0 are missing for R and are wrong for W.

Tags (3)
1 Reply

1,348 Views
Yuri
NXP Employee
NXP Employee

  I will send You JRINTR description from preliminary specs.
It contains the skipped information. 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------