Error in documentation IMX6DQ6SDLSRM.pdf

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error in documentation IMX6DQ6SDLSRM.pdf

2,026件の閲覧回数
frédéric
Contributor III

In the IMX6DQ6SDLSRM.pdf file (mine is 8423886 bytes), page 570 Figure B-112, bits 15 to 0 are missing for R and are wrong for W.

タグ(3)
1 返信

1,316件の閲覧回数
Yuri
NXP Employee
NXP Employee

  I will send You JRINTR description from preliminary specs.
It contains the skipped information. 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------