Epiphany web-browser crashes for pyro

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Epiphany web-browser crashes for pyro

2,864件の閲覧回数
turkersezgin
Contributor III

Hi everyone,

I want to add a web browser to my linux OS which is generated from PYRO branch-yocto project.

Please, can you suggest me sample web browser for open all web pages.?

I tried epiphany but it crashes with these errors;

-Error caching form data: The name org.freedesktop.secrets was not provided by any .service files.

-Error in epiphany: free():invalid pointer: 0x7417d288

-Error retrieving adblock filter: Operation not sopported

Also, I did not bitbake chromium image in my pyro project. Kernel version is 4.1.15

Thanks.

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

2,665件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Turker Sezgin,

If you are using the i.MX6 your best bet would probably be chromium.

If you are using other processors it would depend on its features. For example, the problem with the i.MX7 and chromium would be that the processor does not support OpenGL 2.0 which is required by most current browsers.

I haven’t used epiphany but I would first make sure that it’s a stable release and that its requirements are met.

Regards,

0 件の賞賛
返信

2,665件の閲覧回数
turkersezgin
Contributor III

Hello gusarambula,

Firstly, thanks for your reply.

I am using the i.MX6 quad with yocto PYRO branch. But I can not add chromium in my local.conf. When I add this recipe to local.conf, bitbake operation gives an error.

Also, there is no chromium recipe for pyro branch.

OpenEmbedded Layer Index - recipes 

How can I add chromium to my project?

Please can you help me?

Thanks.

Best regards.

0 件の賞賛
返信