Effect of Deblocking Filter

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Effect of Deblocking Filter

2,767件の閲覧回数
masa-i
Contributor I

I'm checking the effect of deblocking filter in H.264 Encoding on i.MX6.
I've been evaluating the effect by changing  related parameters
  avc_disableDeblk
  avc_deblkFilterOffsetAlpha
  avc_deblkFilterOffsetBeta

In the H.264 encoded stream (I've been checking with analyzing the stream), deblocking filter is  effective.

But the actual effect of the filter can't be confirmed with a decoded image.
(I've checked it by combination of various parameters.)

Did anyone inspect the effect of DBF?

0 件の賞賛
返信
3 返答(返信)

2,598件の閲覧回数
b36401
NXP Employee
NXP Employee

Actually deblocking filter is turned on by default in i.MX6 VPU.

Please refer chapter 69 "Video Processing Unit (VPU)"

of i.MX 6Dual/6Quad Applications Processor Reference Manual for the details.

By the way generally there is no need to change the default setting of 0:0 for alpha:beta

as it gives very good results for a wide range of videos.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,598件の閲覧回数
masa-i
Contributor I

Dear Victor,

Thank you for the information. But I'd like to confirm its effect.

Nothing can confirm the difference in decoding picture in a case with/witout DBF.

Is there a good idea to confirm  effect of DBF ?

regards,

Masahiro

0 件の賞賛
返信

2,598件の閲覧回数
Aemj
Contributor IV

Dear team,

Sorry for rushing you but we still wait for your comment.

BR,

Miyamoto

0 件の賞賛
返信