Eclipse

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Eclipse

1,502 Views
tomgao
Contributor III

when I add new file in the eclipse project . For exmple I add a helloworld project with the yocto plug .And I add a v4l2_modul.c .after reconfigure project the package ,I build the project.But the v4l2_modul.c not be compile .why , how to resolve it ?

0 Kudos
Reply
1 Reply

1,350 Views
igorpadykov
NXP Employee
NXP Employee

Hi tom

one can look at compiler error messages and add necessary

header files which may be missing for v4l2_modul.c. May be

suggested to check

Setting up the Eclipse IDE for Yocto Application Development

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply