ERROR: qtbase-6.5.0-r0 do_configure:

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ERROR: qtbase-6.5.0-r0 do_configure:

ソリューションへジャンプ
3,189件の閲覧回数
gufengzi
Contributor III

according to i.MX Yocto Project User's Guide Rev. LF6.1.36_2.1.0 — 29 September 2023

I run the following commands on ubuntu22.04

qt6 do configure failed.

the openssl version is  1.1.1

can any body help me?

repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-mickledore -m imx-6.1.36-2.1.0.xml

repo sync

DISTRO=fsl-imx-xwayland MACHINE=imx6qdlsabresd source imx-setup-release.sh -b build-xwayland

bitbake imx-image-full

 

| Note: Disabling X11 Accessibility Bridge: D-Bus or AT-SPI is missing.
|
| ERROR: The OpenGL functionality tests failed! You might need to modify the OpenGL package search path by setting the OpenGL_DIR CMake variable to the OpenGL library's installation directory.
|
| CMake Error at cmake/QtBuildInformation.cmake:194 (message):
| Check the configuration messages for an error that has occurred.
| Call Stack (most recent call first):
| cmake/QtBuildInformation.cmake:24 (qt_configure_print_summary)
| cmake/QtBuildInternals/QtBuildInternalsConfig.cmake:514 (qt_print_feature_summary)
| CMakeLists.txt:196 (qt_build_repo_end)
|
|
| -- Configuring incomplete, errors occurred!
| See also "/home/tjt/src/yocto_imx/build-xwayland/tmp/work/cortexa9t2hf-neon-poky-linux-gnueabi/qtbase/6.5.0-r0/build/CMakeFiles/CMakeOutput.log".
| See also "/home/tjt/src/yocto_imx/build-xwayland/tmp/work/cortexa9t2hf-neon-poky-linux-gnueabi/qtbase/6.5.0-r0/build/CMakeFiles/CMakeError.log".
| WARNING: exit code 1 from a shell command.
ERROR: Task (/home/tjt/src/yocto_imx/sources/meta-qt6/recipes-qt/qt6/qtbase_git.bb:do_configure) failed with exit code '1'
WARNING: python3-bcrypt-4.0.1-r0 do_fetch: Failed to fetch URL https://files.pythonhosted.org/packages/source/b/bcrypt/bcrypt-4.0.1.tar.gz;downloadfilename=bcrypt-..., attempting MIRRORS if available

0 件の賞賛
返信
1 解決策
3,151件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @gufengzi!
For iMX6 Quad Plus you have to use "imx6qpsabresd".


To compile with the Yocto Project I always recommend using the machines described on our Yocto User Guide.


You have to create a new Yocto Project for a new machine.
I created a new Yocto Project and I had success on the qtbase compilation (see attached log)


Best Regards!
Chavira

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
3,169件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @gufengzi!
Thank you for contacting NXP Support!

I can replicate the same issue when you set " MACHINE=imx6qdlsabresd ", the target "imx6qdlsabresd" doesn´t exist according to the Yocto Project User Guide.

Changing the machine "imx6qdlsabresd" with "imx6dlsabresd" I don´t see any issue compiling qtbase.

Please try to set a valid machine described on page 7 of the
Yocto Project User Guide

Chavira_0-1704215499678.png

 


Best Regards!
Chavira

0 件の賞賛
返信
3,153件の閲覧回数
gufengzi
Contributor III

I changed the machine "imx6qdlsabresd" with "imx6dlsabresd".

the qtbase issue is not resolved.

the same issue occurs as before.

0 件の賞賛
返信
3,152件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @gufengzi!
For iMX6 Quad Plus you have to use "imx6qpsabresd".


To compile with the Yocto Project I always recommend using the machines described on our Yocto User Guide.


You have to create a new Yocto Project for a new machine.
I created a new Yocto Project and I had success on the qtbase compilation (see attached log)


Best Regards!
Chavira

0 件の賞賛
返信
3,149件の閲覧回数
gufengzi
Contributor III

which version of openssl and ubuntu are you using?

Thanks

0 件の賞賛
返信
3,147件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @gufengzi!

I am using Ubuntu 20.04.6 and OpenSSL 1.1.1f

0 件の賞賛
返信
3,145件の閲覧回数
gufengzi
Contributor III

could you try with ubuntu 22.04?

do you think ubuntu22.04 is ok for this yocto project?

imx yocto project user's guide recommends minimum Ubuntu version is 20.04 or later.

0 件の賞賛
返信
3,165件の閲覧回数
gufengzi
Contributor III

https://github.com/Freescale/meta-freescale/blob/master/conf/machine/imx6qdlsabresd.conf

the github tells me imx6qdlsabresd.conf replaces the following machines:

# * imx6qpsabresd
# * imx6qsabresd
# * imx6dlsabresd
# * imx6solosabresd

so I used imx6qdlsabresd as MACHINE.

the SoC I am using on my board is i.max6quad plus.

May I use imx6dlsabresd as the MACHINE for my board?

Is there any potential problems with different SoC configuration?

Thanks

0 件の賞賛
返信