chavira:~/sabresd$ DISTRO=fsl-imx-xwayland MACHINE=imx6qpsabresd source imx-setup-release.sh -b build-xwayland Build directory is build-xwayland Welcome to Freescale Community BSP The Yocto Project has extensive documentation about OE including a reference manual which can be found at: http://yoctoproject.org/documentation For more information about OpenEmbedded see their website: http://www.openembedded.org/ You can now run 'bitbake ' Common targets are: core-image-minimal meta-toolchain meta-toolchain-sdk adt-installer meta-ide-support Your configuration files at build-xwayland have not been touched. BSPDIR= BUILD_DIR=. meta-freescale directory found chavira:~/sabresd/build-xwayland$ nano conf/local.conf chavira:~/sabresd/build-xwayland$ bitbake -c compile qtbase /usr/lib/python3/dist-packages/html5lib/_trie/_base.py:3: DeprecationWarning: Using or importing the ABCs from 'collections' instead of from 'collections.abc' is deprecated since Python 3.3, and in 3.10 it will stop working from collections import Mapping NOTE: Your conf/bblayers.conf has been automatically updated. Loading cache: 100% | | ETA: --:--:-- Loaded 0 entries from dependency cache. Parsing recipes: 100% |############################################################################################################################################################################| Time: 0:01:13 Parsing of 3440 .bb files complete (0 cached, 3440 parsed). 5303 targets, 431 skipped, 18 masked, 0 errors. NOTE: Resolving any missing task queue dependencies Build Configuration: BB_VERSION = "2.4.0" BUILD_SYS = "x86_64-linux" NATIVELSBSTRING = "ubuntu-20.04" TARGET_SYS = "arm-poky-linux-gnueabi" MACHINE = "imx6qpsabresd" DISTRO = "fsl-imx-xwayland" DISTRO_VERSION = "6.1-mickledore" TUNE_FEATURES = "arm vfp cortexa9 neon thumb callconvention-hard" TARGET_FPU = "hard" meta meta-poky = "HEAD:0a98281d37b0bd8dc1548c390216cb3978e36e0e" meta-oe meta-multimedia meta-python = "HEAD:75cf318cef3b4ee81fad2782cf063ecd69ba8842" meta-freescale = "HEAD:9b00d40b787c2b7105ce209f5635cc1a0cab81ca" meta-freescale-3rdparty = "HEAD:93ba05e3a16a028b770fa1e813b13eb87a59ac63" meta-freescale-distro = "HEAD:b09c18a3f649f0cf1b40432bb39e76ba16fe94e2" meta-bsp meta-sdk meta-ml meta-v2x = "HEAD:6efe87f014c5bdcbda30f06156ee11d8bc3dc7fe" meta-nxp-demo-experience = "HEAD:7f34a32c7877e55e87b6a99e90da4128ed632bf2" meta-arm meta-arm-toolchain = "HEAD:0e043288fd0b17fbf31cf00ae33045107a991144" meta-chromium = "HEAD:e232c2e21b96dc092d9af8bea4b3a528e7a46dd6" meta-clang = "HEAD:af4dcba009ba98250315520f3003fde4ee164cce" meta-gnome meta-networking meta-filesystems = "HEAD:75cf318cef3b4ee81fad2782cf063ecd69ba8842" meta-qt6 = "HEAD:1406d0a85525a71fe5d7892d7f915404290a78ad" meta-parsec meta-tpm = "HEAD:d7db0a3bd1a8639df7570483f003ce00cbe274a2" meta-virtualization = "HEAD:56593e277a377157944a6676e57497066b770a35" Initialising tasks: 100% |#########################################################################################################################################################################| Time: 0:00:02 Sstate summary: Wanted 360 Local 0 Mirrors 0 Missed 360 Current 0 (0% match, 0% complete) NOTE: Executing Tasks NOTE: Tasks Summary: Attempted 1687 tasks of which 0 didn't need to be rerun and all succeeded. chavira:~/sabresd/build-xwayland$