ENET & RGMII

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ENET & RGMII

2,312 Views
eliaz
Contributor II

Hi ,

I'm Intending to use  RGMII periphery, Does NVCC_ENET and NVCC_RGMII  must be tied to the same supply ?

 In the SABRE schematics I see that MDC from ENET is going to the RGMII PHY so which voltage does it take ? 

Regards, 

Eli

Labels (1)
0 Kudos
Reply
2 Replies

2,153 Views
jamesbone
NXP TechSupport
NXP TechSupport

Yes,  NVCC_ENET and NVCC_RGMII  can be attach both to the same power supply if the PHY that you are planning to use it is using the same power levels. It can be different since NVCC_ENET it is refer to the Ethernet Controller + Phy and NVCC_RGMII it is only for the Ethernet Controller no internal Phy to use.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,153 Views
eliaz
Contributor II

?

0 Kudos
Reply