ENET & RGMII

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ENET & RGMII

2,238件の閲覧回数
eliaz
Contributor II

Hi ,

I'm Intending to use  RGMII periphery, Does NVCC_ENET and NVCC_RGMII  must be tied to the same supply ?

 In the SABRE schematics I see that MDC from ENET is going to the RGMII PHY so which voltage does it take ? 

Regards, 

Eli

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,079件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Yes,  NVCC_ENET and NVCC_RGMII  can be attach both to the same power supply if the PHY that you are planning to use it is using the same power levels. It can be different since NVCC_ENET it is refer to the Ethernet Controller + Phy and NVCC_RGMII it is only for the Ethernet Controller no internal Phy to use.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,079件の閲覧回数
eliaz
Contributor II

?

0 件の賞賛
返信