EIM write speed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EIM write speed

4,298件の閲覧回数
hyunhoshin
Contributor III

I'm using EIM to connect with ADV212(HW jpeg 2000 encoder)

but, EIM write speed is too slow..

below attach file("EIM_WRITE_CS_WAVEFORM.png") is EIM's chip select waveform

I think first CS enable to second CS enable period is too large(long time)

I don't know why?

Anyone know this situation?

 

*Test code(infinite write loop)

 

#define PIXEL              0x0

adv_reg = ioremap(0x8000000,(0x8000000-4));// 128MB area

pixel_addr = adv_reg+(PIXEL*0x00400000/2);

while(1)

{

     *pixel_addr = 0xAA;

}

*EIM setting values

static void setup_weimcs(void)

{

     unsigned int reg;

     void __iomem *nor_reg = MX6_IO_ADDRESS(WEIM_BASE_ADDR);      //0x021B_8000

     void __iomem *ccm_reg = MX6_IO_ADDRESS(CCM_BASE_ADDR);

     /*CCM_BASE_ADDR + CLKCTL_CCGR6*/

     reg = readl(ccm_reg + 0x80);

     reg |= 0x00000C00;

     writel(reg, ccm_reg + 0x80);

     __raw_writel(0x00000020, nor_reg + 0x090);

     __raw_writel(0x000109B9, nor_reg + 0x000);

     __raw_writel(0x00001000, nor_reg + 0x004);

     __raw_writel(0x08001100, nor_reg + 0x008);//read timing

     __raw_writel(0x00000000, nor_reg + 0x00C);

     __raw_writel(0x02000240, nor_reg + 0x010);//write timing

}

ラベル(1)
タグ(4)
0 件の賞賛
返信
3 返答(返信)

3,066件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Shin,

    Please notice here :

while(1)

{

     *pixel_addr = 0xAA;

}

I think issue should be generated here. It maybe take up all times of CPU. and cpu has no time to handle other tasks.

3,066件の閲覧回数
kartjon
Contributor I

can you help me? I do not know why the EIM do not wor on my board.Pin by the oscilloscope, no change. I config and write EIM like the following:

1.config MUX and PAD

static iomux_v3_cfg_t mx6q_sabresd_pads[] = {

                    .

                    .

                    .

/* eim */

        MX6Q_PAD_EIM_OE__WEIM_WEIM_OE,

        MX6Q_PAD_EIM_RW__WEIM_WEIM_RW,

        MX6Q_PAD_EIM_WAIT__WEIM_WEIM_WAIT,

        MX6Q_PAD_EIM_LBA__WEIM_WEIM_LBA,

        MX6Q_PAD_EIM_BCLK__WEIM_WEIM_BCLK,

        MX6Q_PAD_EIM_CS0__WEIM_WEIM_CS_0,

        /* Data Bus */

        MX6Q_PAD_EIM_D16__WEIM_WEIM_D_16,

        MX6Q_PAD_EIM_D17__WEIM_WEIM_D_17,

        MX6Q_PAD_EIM_D18__WEIM_WEIM_D_18,

        MX6Q_PAD_EIM_D19__WEIM_WEIM_D_19,

        MX6Q_PAD_EIM_D20__WEIM_WEIM_D_20,

        MX6Q_PAD_EIM_D21__WEIM_WEIM_D_21,

        MX6Q_PAD_EIM_D22__WEIM_WEIM_D_22,

        MX6Q_PAD_EIM_D23__WEIM_WEIM_D_23,

        MX6Q_PAD_EIM_D24__WEIM_WEIM_D_24,

        MX6Q_PAD_EIM_D25__WEIM_WEIM_D_25,

        MX6Q_PAD_EIM_D26__WEIM_WEIM_D_26,

        MX6Q_PAD_EIM_D27__WEIM_WEIM_D_27,

        MX6Q_PAD_EIM_D28__WEIM_WEIM_D_28,

        MX6Q_PAD_EIM_D29__WEIM_WEIM_D_29,

        MX6Q_PAD_EIM_D30__WEIM_WEIM_D_30,

        MX6Q_PAD_EIM_D31__WEIM_WEIM_D_31,

        /* Address Bus */

        MX6Q_PAD_EIM_DA15__WEIM_WEIM_DA_A_15,

        MX6Q_PAD_EIM_DA14__WEIM_WEIM_DA_A_14,

        MX6Q_PAD_EIM_DA13__WEIM_WEIM_DA_A_13,

        MX6Q_PAD_EIM_DA12__WEIM_WEIM_DA_A_12,

        MX6Q_PAD_EIM_DA11__WEIM_WEIM_DA_A_11,

        MX6Q_PAD_EIM_DA10__WEIM_WEIM_DA_A_10,

        MX6Q_PAD_EIM_DA9__WEIM_WEIM_DA_A_9,

        MX6Q_PAD_EIM_DA8__WEIM_WEIM_DA_A_8,

        MX6Q_PAD_EIM_DA7__WEIM_WEIM_DA_A_7,

        MX6Q_PAD_EIM_DA6__WEIM_WEIM_DA_A_6,

        MX6Q_PAD_EIM_DA5__WEIM_WEIM_DA_A_5,

        MX6Q_PAD_EIM_DA4__WEIM_WEIM_DA_A_4,

        MX6Q_PAD_EIM_DA3__WEIM_WEIM_DA_A_3,

        MX6Q_PAD_EIM_DA2__WEIM_WEIM_DA_A_2,

        MX6Q_PAD_EIM_DA1__WEIM_WEIM_DA_A_1,

        MX6Q_PAD_EIM_DA0__WEIM_WEIM_DA_A_0,

};

2.set EIM register

static void mx6q_setup_eim_cs(void)

{

    void __iomem *ram_reg = MX6_IO_ADDRESS(WEIM_BASE_ADDR);

    void __iomem *ccm_reg = MX6_IO_ADDRESS(CCM_BASE_ADDR);

    unsigned int reg;

    struct clk *clk;

    u32 rate;  

    /* CLKCTL_CCGR6: Set emi_slow_clock to be on in all modes */

    reg = readl(ccm_reg + 0x80);

    reg |= 0x00000C00;

    writel(reg, ccm_reg + 0x80);

    clk = clk_get(NULL, "emi_slow_clk");

    if (IS_ERR(clk))

        printk(KERN_ERR "emi_slow_clk not found\n");

    rate = clk_get_rate(clk);

    if (rate != 132000000)

        printk(KERN_ERR "Warning: emi_slow_clk not set to 132 MHz!"

               " WEIM NOR timing may be incorrect!\n");

    writel(0x403304b1, ram_reg);

    writel(0x0, ram_reg + 0x4);

    writel(0x0f010000, ram_reg + 0x8);

    writel(0x00000008, ram_reg + 0xc);

    writel(0x0f040040, ram_reg + 0x10);

    writel(0x00000000, ram_reg + 0x14);

    writel(0x00000000, ram_reg + 0x90);

}

3.iomap(addr:0x08000000, size:0x02000000)

weim->base = devm_ioremap(&pdev->dev, res->start ,len);

            if (weim->base == NULL) {

                    dev_err(&pdev->dev, "Failed to ioremap flash region\n");

                    ret = -EIO;

                    goto weim_err;

            }

4.read and write EIM

long EIM_ioctl(struct file* pFile, unsigned int cmd, unsigned long data)

{

    int val = 0;

    struct eimNode* node = (struct eimNode*)data;

    int *addr = 0; 

    if(weim == 0)

        return FAIL;

    switch(cmd)

    {

    case EIM_READ:

        val = __raw_readl(weim->base + node->offset);

        node->data = val;

        break;

    case EIM_WIRTE:

        __raw_writel(node->data, weim->base + node->offset);

        break;

    default:

        break;

    }

    return SUCCESS;

}

0 件の賞賛
返信

3,066件の閲覧回数
hyunhoshin
Contributor III

blow code is test code to test EIM write

while(1)

{

     *pixel_addr = 0xAA;

}

pixel_addr pointer is address space of EIM, so continuing write to EIM without any other processing.

0 件の賞賛
返信