EIM_EB3 boot configuration pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EIM_EB3 boot configuration pin

ソリューションへジャンプ
34,940件の閲覧回数
rowangifford
Contributor II

I think there may be an error in the IMX6Q reference manual regarding one of the boot configuration pins.

From the IMX6Q reference manual page 269 pin EIM_EB3 is linked to boot configuration BOOT_CFG3[1]. Other pages also reference this (Table 4-2 page 327), Page 1974 IOMUXC_SW_MUX_CTL_PAD_EIM_EB3_B field descriptions.

However Table 8-3 on page 384 states EIM_EB3 is linked to BOOT_CFG4[7].

BOOT_CFG4[7] makes more sense as it is linked to the infinite loop test, whereas BOOT_CFG3[1] is reserved.

Which is correct?

Thanks,

Rowan

ラベル(1)
0 件の賞賛
返信
1 解決策
1,845件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rowan

yes, correct is Table 8-3 on page 384.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,846件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rowan

yes, correct is Table 8-3 on page 384.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------