ECSPI using SDMA for cortex M4 can not recive data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ECSPI using SDMA for cortex M4 can not recive data

4,024 Views
JanChiang
Contributor I

Hi ,

I have a strange problem. I use SDMA to control the SPI according to the example ecspi_polling_master. Finally, I can get the correct data(tx and rx) on the oscilloscope, but the data from the ecspi_receiveData interface is always 0(rx).

The ECSPI Control Register is 0xF0B211, The Config Register is 0x100011

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

4,020 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jan

 

I believe for sdma "polling" should not be used, for m4 ecspi sdma example one can look at

 

Best regards
igor

0 Kudos
Reply

4,011 Views
JanChiang
Contributor I

and here is the ecspi api for our platform 

0 Kudos
Reply

3,973 Views
igorpadykov
NXP Employee
NXP Employee

right, in your release such examples are not available, you can use them just as reference for

creating own.

 

Best regards
igor

0 Kudos
Reply

4,012 Views
JanChiang
Contributor I

Hi igor:

thanks your reply, But our platform and the files you provided look very different, the interface mentioned in your files can not be found in our code

0 Kudos
Reply