Section 4.1 of AN4397, last paragraph:
"The fourth difference is about SATA_VP (G13) and SATA_VPH (G12). In i.MX 6Quad and i.MX 6Dual, SATA_VP and SATA_VPH are recommended to be grounded, if not in use. In i.MX 6DualLite and i.MX 6Solo, no SATA function is available and all these pins are recommended to be NC."
If G12 and G13 are NC on the DualLite, can they be powered, i.e. no need for a selection resistor when using the DualLite vs. Quad?