Dual OpenGL application v-sync issue on i.MX6Q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dual OpenGL application v-sync issue on i.MX6Q

3,053件の閲覧回数
frankchenmh
Contributor III

Hi, we got an issue about i.MX6 dual OpenGL applications (render to two framebuffers).

Customer board based on i.MX6Q sabresd.
Linux BSP
GPU driver and sdk: L3.0.35_4.0.0

fb0: PAL TVout, refresh rate 50Hz
fb2: HDMI, refresh rate 60Hz

OpenGL app1: render to fb0
OpenGL app2: render to fb2

The OpenGL applications are developed based on the samples in gpu_sdk_v1.00.tar.gz.

When the OpenGL applications render frames, the frames are synced with framebuffer v-sync. So the applications can run at the framerate same to the framebuffer refresh rate. When run app1 only, we can see that the app1 frame rate is 50Hz. When run app2 only, we can see the app2 frame rate is 60Hz.

However if we run both app1 and app2, the framerate of app1 and app2 are both 50Hz no matter which app is started first. The app2 is synced with fb0 but not fb2. This is incorrect.

For example:
Step 1) Run app2. And we can see the frame rate of app2 is 60Hz.
Step 2) Run app1. Now the frame rate of app2 changes to 50Hz.

Please help on how to fix this issue. Thanks!

4 返答(返信)

2,882件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Frank,

This is fixed on the new driver of the GPU you need to upgrade since we have not porting this driver to L3.0.35.

Regards

2,882件の閲覧回数
frankchenmh
Contributor III

Hi,

Thanks for your reply!

From which version of the BSP the GPU driver was updated to fix the issue? I'll check if it can be back ported to the BSP that I used.

Or is there any standalone patch for this fix?

0 件の賞賛
返信

2,882件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

The fixed appear in L4.9.88 BSP version.

0 件の賞賛
返信

2,882件の閲覧回数
frankchenmh
Contributor III

Thanks! I'll check the driver in the BSP version you mentioned.

0 件の賞賛
返信