It is mentioned on the NXP website that Silex is a proven partner (NXP - Partner Profile Information ). One of the supported devices is the SX-PCEAC2 WiFi module with QCA6174-5 chip. Two questions:
Hi Hans
it is supported in NXP Linux 4.9.88, one can look in Linux Manual included in
Linux 4.9.88_2.0.0 BSP & Multimedia Codecs Documentation
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
This is a bit confusing:
- the documentation that you are referring to is about the QCA CLD driver
- in the article How to evaluate QCA6174 radio on i.MX 8 EVK platform?, the ath10k driver is used.
These aren't the same drivers. NXP supports the same chip with different drivers ?
Best regards,
Hans
Hi Hans
below part of L4.9.88_2.0.0 Release Notes
could you point where in official documentation "QCA CLD driver" mentioned.
May be also useful to check murata wifi imx portal:
wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html
Article is just another solution, note nxp official documents are located on
Best regards
igor
Hi Igor,
QCA CLD is mentioned in the i.MX Reference Manual (Document IMXLXRM, Rev. L.4.9.88_2.0.0-ga, 05/2018), section 4.12.2.
Best regards,
Hans