Does the iMX6 Solox SDK include the PCIe protocol stack for Endpoint?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the iMX6 Solox SDK include the PCIe protocol stack for Endpoint?

1,833 Views
infantjesurajfr
Contributor I

I will be using the iMX6 Solox processor in my design which will be a PCIe endpoint system.

Does the iMX6 Solox SDK include the PCIe protocol stack for Endpoint?

Tags (2)
0 Kudos
Reply
2 Replies

1,645 Views
Bharath_R
Contributor I

Hello James,

I am using IMX6 Dual lite processor, can I use SDK for PCIe test.

if yes, can i get test procedure.

Thanks and Regards,

Bharath R

0 Kudos
Reply

1,749 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Infant,

Nop, the PCIe Module it is not available in the SDK,  you can try using the Linux BSP provided by NXP, that includes the PCIe  Endpoint Core,.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply