Does the iMX6 Solox SDK include the PCIe protocol stack for Endpoint?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the iMX6 Solox SDK include the PCIe protocol stack for Endpoint?

1,902件の閲覧回数
infantjesurajfr
Fresh Out Contributor

I will be using the iMX6 Solox processor in my design which will be a PCIe endpoint system.

Does the iMX6 Solox SDK include the PCIe protocol stack for Endpoint?

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,714件の閲覧回数
Bharath_R
Contributor I

Hello James,

I am using IMX6 Dual lite processor, can I use SDK for PCIe test.

if yes, can i get test procedure.

Thanks and Regards,

Bharath R

0 件の賞賛
返信

1,818件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Infant,

Nop, the PCIe Module it is not available in the SDK,  you can try using the Linux BSP provided by NXP, that includes the PCIe  Endpoint Core,.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信