Does somebody have cx20709 codec alsa driver source code ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does somebody have cx20709 codec alsa driver source code ?

4,416件の閲覧回数
wenmingfeng
Contributor III

I want to use cx20709 codec on imx.6 dual lite customer board, does someone has cx20709 codec driver? please share me the link or where can I get it.

Thanks aheard!

w.F.

0 件の賞賛
返信
2 返答(返信)

2,834件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi wenming

I am not aware of these drivers by it may be useful to check

Chapter 8 Porting Audio Codecs to a Custom Board attached porting guide

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,834件の閲覧回数
wenmingfeng
Contributor III

Thanks Igor,

Since I remember on imx early than 5 in the reference board, they had used conexant codec chips, now they use wmxxx/. If there is source code, then nice to have.

regards!

wfeng

0 件の賞賛
返信