Does it support USB3.0 driver using i.MX53 on MFG tool?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does it support USB3.0 driver using i.MX53 on MFG tool?

1,751 次查看
StanleyLee
NXP Employee
NXP Employee

This is a question raised by one customer.

Currently when Mobis use the MFG tool on Laptop with USB3.0 driver, it can't search the USB port on MFG tool. And then MFG tool is down the program on Laptop.

 

 

[Answer] The functionality will be implemented in Mfgtool2.0.

0 项奖励
回复
3 回复数

1,228 次查看
compmas2
Contributor V

The answer of it will be implemented in MfgTool 2.0 is not an acceptable answer since MfgTool 2.0 does not support the i.MX53.  How is someone using an i.MX53 with a PC containing all USB 3.0 ports supposed to use the MfgTool?

0 项奖励
回复

1,228 次查看
maciejkaczmarcz
Contributor I

If anyone will struggle with this problem, the workaround is disable usb 3.0 support in BIOS settings. All USB ports will be visible as 2.0 and MFG tool will work as it should (at least in my case)

Best regards

0 项奖励
回复

1,228 次查看
Yuri
NXP Employee
NXP Employee

There is MFG, supporting USB3

0 项奖励
回复