Does imx93 support WDQS?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does imx93 support WDQS?

跳至解决方案
489 次查看
takayuki_ishii
Contributor IV

Hello community,

 

I have one question about i.MX93 DDR PHY function.

Does i.MX93 support WDQS?

 

In following thread, it say that i.MX8M Plus support WDQS when WDQSEXTENSION is enabled.

https://community.nxp.com/t5/i-MX-Processors/Is-IMX8M-Plus-using-WDQS/m-p/1877743

 

But, it have no WDQSEXTENSION bit in i.MX93.

Does it have another method to "write and masked write operation DQS control"?

 

Best regards,

Ishii.

 

0 项奖励
回复
1 解答
457 次查看
pengyong_zhang
NXP Employee
NXP Employee

HI, @takayuki_ishii 

i.MX93 support WDQS feature.

B.R

在原帖中查看解决方案

0 项奖励
回复
2 回复数
212 次查看
bernhardfink
NXP Employee
NXP Employee

We don't document the registers of the DDRC PHY, but for this specific feature (in fact this is a requirement of JESD209-4B) you find at least an indication that it is enabled:

bernhardfink_0-1726227597651.png

In the lpddr4x_timing.c file you can't identify this bit without having a detailed description of the registers, but as Pengyong wrote, it is enabled by default.

Regards,
Bernhard.

0 项奖励
回复
458 次查看
pengyong_zhang
NXP Employee
NXP Employee

HI, @takayuki_ishii 

i.MX93 support WDQS feature.

B.R

0 项奖励
回复