Does i.MX6ULL Support Windows IoT Core?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.MX6ULL Support Windows IoT Core?

4,877 Views
ScottKerstein
Contributor III

According to Windows Embedded PSB page: https://www.microsoft.com/windowsembedded/en-us/bspcatalog.aspx, i.MX 6ULL is not being used for any Windows Embedded Compact (CE) OS.

Can you please confirm i.MX 6ULL compatibility with Window CE OS?

 

According to this table, found in:  https://msdn.microsoft.com/en-us/windows/hardware/commercialize/design/minimum/minimum-hardware-requ..., i.MX 6ULL can support IoT core.

Can you please confirm i.MX 6ULL can support Windows IoT Core?

Thank you in advance,

Scott

 

Labels (2)
0 Kudos
Reply
7 Replies

3,476 Views
ChiragShah
Contributor I

Microsoft and NXP announced this week that Windows 10 IoT Core will support the i.MX6 and i.MX7 families

https://blogs.microsoft.com/iot/2018/02/27/enabling-iot-solutions-will-last-long-term/

0 Kudos
Reply

3,476 Views
ScottKerstein
Contributor III

Hello Yuri,

Technically speaking the part could support Window IoT is a port did exist from a 3rd Party, right?  I'm not asking if NXP provides a BSP.

0 Kudos
Reply

3,476 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Basically - yes, i.MX 6ULL can support Windows IoT. (Based on the requirements 
on the following page Learn About Windows 10 IoT Core | Windows IoT )

Regards,

Yuri.

0 Kudos
Reply

3,476 Views
ScottKerstein
Contributor III

Hello Yuri,

Will i.MX6ULL support WEC2013?

Thanks,

Scott

0 Kudos
Reply

3,476 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I did not find WEC2013 minimal hardware requirements, except that
Windows Embedded Compact 2013 requires that ARM CPUs support the

ARM v7 as well as Thumb2 opcode sets. The i.MX6 ULL meets it.

But I am not aware about any WEC2013 implementation on i.MX6ULL.

Regards,

Yuri.

0 Kudos
Reply

3,476 Views
Yuri
NXP Employee
NXP Employee

Hello

NXP does not support Windows CE / IoT.  You may apply to third firms.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 Kudos
Reply

3,476 Views
ScottKerstein
Contributor III

Hello Yuri,

From a technical standpoint, the part could support Windows IoT at the hardware level if a BSP existed from a 3rd party, right?

Thanks.

0 Kudos
Reply