Does gpu Z160 support a buffer lager than 2048x2048 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does gpu Z160 support a buffer lager than 2048x2048 ?

跳至解决方案
924 次查看
sparkzh
Contributor I

I am working on a board based on imx53. What I am doing is to support xrandr dual display on it. Clone mode works well. But when it comes to extend mode, there is something strange as the picture shows.

QQ截图20130712172009.jpg

extend mode: hdmi + lvds

     hdmi: 1920x1080

     lvds:     800x480

     pos:     hdmi right-of lvds

1. If the summary of the width of the two outputs is larger than 2048, the display appears abnormal.

     If EXA is disabled, dual display works well.  Does anyone have met something similar before?

2. In Z160.h:

     /* Largest buffer is 2048x2048 */

     #define Z160_MAX_WIDTH 2048

     #define Z160_MAX_HEIGHT 2048

     Does gpu z160 support a buffer larger than 2048x2048 ?

Any advice is appreciated.

Thank you in advance.

标记 (4)
0 项奖励
回复
1 解答
803 次查看
PrabhuSundarara
NXP Employee
NXP Employee

It does not support larger than 2048x2048. 2048x2048 is the max.

在原帖中查看解决方案

0 项奖励
回复
1 回复
804 次查看
PrabhuSundarara
NXP Employee
NXP Employee

It does not support larger than 2048x2048. 2048x2048 is the max.

0 项奖励
回复