Does g2d support G2D_RGB888 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does g2d support G2D_RGB888 ?

2,718 Views
brenhale
Contributor I

The G2D API format enumeration describes G2D_RGB888 as a 24-bit RGB option (enum #10).

However attempts to use this, even for very simple blit operation yield errors for either invalid src or dst format.

g2d_blit_2d: Invalid src format 10!

There is no errata for lack of support for this. Should it work?

Tested on imx8mm.

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

2,598 Views
michaelnazzaren
Contributor I

Hi

I have the same problem. Can we have a folowup? Android 10 is my bsp base on

int ret;
void* g2dHandle = getHandle();
struct g2d_buf s_buf, d_buf;
struct g2d_surface s_surface, d_surface;

s_buf.buf_paddr = tmpBuf.mPhyAddr;
s_buf.buf_vaddr = tmpBuf.mVirtAddr;
d_buf.buf_paddr = dstBuf.mPhyAddr;
d_buf.buf_vaddr = dstBuf.mVirtAddr;

s_surface.format = G2D_RGB888;
s_surface.planes[0] = (long)s_buf.buf_paddr;
s_surface.left = 0;
s_surface.top = 0;
s_surface.right = src->width();
s_surface.bottom = src->height();
s_surface.stride = src->width();
s_surface.width = src->width();
s_surface.height = src->height();
s_surface.rot = G2D_ROTATION_0;

d_surface.format = (g2d_format)convertPixelFormatToG2DFormat(dst->format());
d_surface.planes[0] = (long)d_buf.buf_paddr;
d_surface.planes[1] = (long)d_buf.buf_paddr + dst->width() * dst->height();
d_surface.left = 0;
d_surface.top = 0;
d_surface.right = dst->width();
d_surface.bottom = dst->height();
d_surface.stride = dst->width();
d_surface.width = dst->width();
d_surface.height = dst->height();
d_surface.rot = G2D_ROTATION_0;

ret = mBlitEngine(g2dHandle, (void*)&s_surface, (void*)&d_surface);
if (ret == 0) {
mFinishEngine(g2dHandle);
}

0 Kudos
Reply

2,307 Views
joanxie
NXP TechSupport
NXP TechSupport

confirmed that imx8mm doesn't support this, only imx8qxp and imx8qm support this format

0 Kudos
Reply

2,651 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the gpu api, gpu should support this format, but what's your case? did you capture video as rgb888 from camera?

0 Kudos
Reply