Does each imx28 comes with it's own unique MAC address?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does each imx28 comes with it's own unique MAC address?

跳至解决方案
1,022 次查看
JeromeBaron
Contributor II

Hi everyone,

I'm a bit confused about the MAC address in the imx28. I saw that a user can write it's own address by changing the HW_OCOTP_CUSTx register. I also know where this is changed in the code.

But, what about a fresh new device, is it supposed to come with it's own "freescale" MAC address? If I want to develop a product that use it, do I have to buy a MAC pool or I can use the freescale one?

Regards,

Jerome

标签 (1)
0 项奖励
回复
1 解答
862 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Jerome,

No they do not come with a MAC address, you need to buy it separately:

http://en.wikipedia.org/wiki/Organizationally_Unique_Identifier


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
863 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Jerome,

No they do not come with a MAC address, you need to buy it separately:

http://en.wikipedia.org/wiki/Organizationally_Unique_Identifier


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
862 次查看
JeromeBaron
Contributor II

Wow, that's a bummer.

0 项奖励
回复