Does each imx28 comes with it's own unique MAC address?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does each imx28 comes with it's own unique MAC address?

ソリューションへジャンプ
971件の閲覧回数
JeromeBaron
Contributor II

Hi everyone,

I'm a bit confused about the MAC address in the imx28. I saw that a user can write it's own address by changing the HW_OCOTP_CUSTx register. I also know where this is changed in the code.

But, what about a fresh new device, is it supposed to come with it's own "freescale" MAC address? If I want to develop a product that use it, do I have to buy a MAC pool or I can use the freescale one?

Regards,

Jerome

ラベル(1)
0 件の賞賛
返信
1 解決策
811件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Jerome,

No they do not come with a MAC address, you need to buy it separately:

http://en.wikipedia.org/wiki/Organizationally_Unique_Identifier


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
812件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Jerome,

No they do not come with a MAC address, you need to buy it separately:

http://en.wikipedia.org/wiki/Organizationally_Unique_Identifier


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
811件の閲覧回数
JeromeBaron
Contributor II

Wow, that's a bummer.

0 件の賞賛
返信