Does each imx28 comes with it's own unique MAC address?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does each imx28 comes with it's own unique MAC address?

Jump to solution
1,031 Views
JeromeBaron
Contributor II

Hi everyone,

I'm a bit confused about the MAC address in the imx28. I saw that a user can write it's own address by changing the HW_OCOTP_CUSTx register. I also know where this is changed in the code.

But, what about a fresh new device, is it supposed to come with it's own "freescale" MAC address? If I want to develop a product that use it, do I have to buy a MAC pool or I can use the freescale one?

Regards,

Jerome

Labels (1)
0 Kudos
Reply
1 Solution
871 Views
SergioSolis
NXP Employee
NXP Employee

Hello Jerome,

No they do not come with a MAC address, you need to buy it separately:

http://en.wikipedia.org/wiki/Organizationally_Unique_Identifier


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
872 Views
SergioSolis
NXP Employee
NXP Employee

Hello Jerome,

No they do not come with a MAC address, you need to buy it separately:

http://en.wikipedia.org/wiki/Organizationally_Unique_Identifier


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
871 Views
JeromeBaron
Contributor II

Wow, that's a bummer.

0 Kudos
Reply