Does bootloader detect CD/DATA3 micro sd card?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does bootloader detect CD/DATA3 micro sd card?

Jump to solution
6,324 Views
MehmetAliIpin
Contributor V

Dear Sir,

 

We have an i.mx6 board which is based on mx6sabresd kit. We can download u-boot with USB loader.

and I modified u-boot to detect and run SD card for 4 bit interface.

 

Our SD card is micro 4 bit wide SD and its card detect pin is also different (CD/DATA3) from origininal kit design. For the small PCB sizes, there is no boot config switches or resistors also. Therefore we will program the fuses to processor to boot from SD card, (or (Q)SPI flash).

 

I wonder if mx6 boot loader firmware checks for special sd card detect pins and/or if not find a card, does it check CD/DATA3 pins status for u-boot code? do we need any pull up/pull down resistor for this pin to be detected?

 

Could Anybody help?

 

Thanks and best regards.

 

Mehmet Ali

Labels (3)
1 Solution
5,883 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mehmet

 

yes ROM does not check CD/DATA3, CD is only checked for

interfaces described in Table 8-17. SD/MMC IOMUX pin configuration

i.MX6DQ Reference Manual or relevant processor Boot Chapter Reference Manual.

Best regards
igor

View solution in original post

0 Kudos
Reply
6 Replies
5,883 Views
mehmetipin
Contributor II

Dear Igor

Thank you very much.

Best regards.

0 Kudos
Reply
5,883 Views
mehmetipin
Contributor II

Dear Igor,

I checked the boot_cfg[7:5] bits of efuse configuration register, see that 4 bit is supported,

does it mean, boot loader will not check the CD/DATA3 pin in 4 bit mode (there is no special card detect pin in 4 bit SD card) , and continue to check other u-boot loading tasks from 4 bit SD card as shown in figures 8-10 thr. 8.15 in ref manual, if we program the efuse boot register accordingly?

Best regards

0 Kudos
Reply
5,884 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mehmet

 

yes ROM does not check CD/DATA3, CD is only checked for

interfaces described in Table 8-17. SD/MMC IOMUX pin configuration

i.MX6DQ Reference Manual or relevant processor Boot Chapter Reference Manual.

Best regards
igor

0 Kudos
Reply
5,883 Views
lokesh
Contributor II

Here is what I have checked on the board that I have. I have flashed u-boot on SD Card and the u-boot boots fine, irrespective of the Carrier Detect (CD). However, u-boot does have MUX setting of the GPIO pins for SD Card Detect and it will be used when it will check the file system for booting kernel.  If the SD Card Detect is not set properly, it will not list the file system ( for example, when  using ext2ls).

I have put some more details in the link below, if you want to check

Using SABRE-SD u-boot on Sabre Lite for i.MX6 | Reference Designer  

5,883 Views
MehmetAliIpin
Contributor V

Dear Vikas,

Thank you very much for your answer.

Best regards.

0 Kudos
Reply
5,883 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mehmet

ROM does not check CD/DATA3, CD is checked for

interfaces described in Table 8-17. SD/MMC IOMUX pin configuration

i.MX6DQ Reference Manual or relevant processor Boot Chapter Reference Manual.

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply